Post Go back to editing

input filter capacitor value

Category: Hardware
Product Number: AD4630-24

Hi,

in datasheet

Figure 41. Typical Application Circuit Diagrams.

When input is driven with differential amp ADA4945-1, there is 270pF connected between IN0+ and IN0-, but when the input is driven by ADA4896, there is no such differential capacitor, why?

And why the capacitor value between IN0+ to GND, and IN0- to GND is 560pF, but the differential cap between IN0+ and IN0- is 270pF, how to calculate the right value for these capacitors?