Post Go back to editing

About the internal resistance of the max1032 analog input circuit

Thread Summary

The user inquired about the resistance values of R1 and R2 in the Simplified Analog Input Circuit for the MAX1032, noting the input resistance RCH_ is 17kΩ (typ). The final answer directed the user to visit the Analog Devices technical support pages for further assistance. Another user echoed the same question, emphasizing the need for R1 and R2 values to understand the calculation of Vsj as described in the datasheet.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX1032

Hi,

My customer is considering the MAX1032.

It says that "Input Resistance RCH_" is 17kΩ (typ), but

could you tell me about the resistance values ​​of R1 and R2 in Figure 6. Simplified Analog Input Circuit?

www.analog.com/.../MAX1032-MAX1033.pdf

Best Regards,

Naohisa

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.