Post Go back to editing

NOT getting any response from AD7730

Category: Software
Product Number: AD7730

hey I an using ad7730 for getting the load cell reading but I am not receiving any data , I have tried the pseudo code given in the data sheet , when i checked with logic analyzer the data is correct in MOSI but nothing comming in MISO.

my POL pin is high and in the controller i am using clock polarity HIGH and clock phase as 2 EDGE can someone provide clarification in this ?

void AD7730_Start_Cont_Read(AD7730 gauge){

spi_tx_buffer[0] = 0x02;//CR_SINGLE_WRITE | CR_MODE_REGISTER; //write to comms register and set next write to mode reg

Tx_AD7730(1, spi_tx_buffer); //0x02

spi_tx_buffer[0] = 0x21;//MR1_MODE_CONTINUOUS | CURRENT_MODE_1_SETTINGS_READ; //write to mode reg startin cont readings for 0-10mV range

spi_tx_buffer[1] = 0x80; //CURRENT_MODE_0_SETTINGS_READ;

Tx_AD7730(2, spi_tx_buffer); //0x2180

spi_tx_buffer[0] = 0x21; //CR_CONTINUOUS_READ_START | CR_DATA_REGISTER;

Tx_AD7730(1, spi_tx_buffer); //0x21

while(AD7730_ConfigData->AD7730_dataReadyPin_read() != GPIO_PIN_RESET); //wait for ready pin to go low after calibration //wait for ready pin to go low when cont readings start

CONT_READ_STARTED = SET;

}

void AD7730_Read_Cont(AD7730 gauge, uint8_t * rx_buffer){

spi_tx_buffer[0] = 0x0;

spi_tx_buffer[1] = 0x0;

spi_tx_buffer[2] = 0x0; //need to transfer all 0 bytes to keep DIN of AD7730 low prevent device reset during cont read

while(AD7730_ConfigData->AD7730_dataReadyPin_read() != GPIO_PIN_RESET); //wait for ready pin to go low after calibration //wait for ready pin to go low

AD7730_ConfigData->AD7730chipSelectSET(); //slave select low to begin

BSP_Delay(1);

AD7730_ConfigData->BSP_AD7730_SPI_TransmitReceive((uint8_t *)spi_tx_buffer,(uint8_t *)rx_buffer,3,1000);

BSP_Delay(1);

AD7730_ConfigData->AD7730chipSelectReset(); //slave select low to begin

}

void AD7730_Stop_Cont_Read(AD7730 gauge){

spi_tx_buffer[0] = CR_SINGLE_WRITE | CR_CONTINUOUS_READ_STOP; //0x30

Tx_AD7730(1, spi_tx_buffer);

CONT_READ_STARTED = RESET;

}

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.