Post Go back to editing

Maximum input voltage

Category: Datasheet/Specs
Product Number: EVAL-AD7608, AD7608

Hey,

I have a development AD7608 development board, the datasheet specifies that the board requires a input voltage between 7 and 9 V.
When looking on the schematic it seems like the inputs are connected to two different capacitors (C23, C24), a voltage divider and the VIN of the ADP7104ARDZ-5.0 chip.

Based on the BOM for the AD7608 eval kit, the capacitors have a rating of 16 and 50 V.

Based on the datasheet of the ADP7104ARDZ-5.0, VIN can range between 3.3 V and 20 V. and the Enable pin can be anything from -0.3 V to VIN (relative to ground).

What is it that decided the voltage range of 7-9 V on the development board, what is it that stops me from being able to connect 12 V on the input (connector J3).

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.