Post Go back to editing

AD7091 return wrong value

Category: Hardware
Product Number: AD7091

Hi.

I apologize in advance for the bad english.

I'm developing with AD7091.

My problem is ADC gives wrong value.

And If I get data more often, peak points appears.

VDD is 5V.

When input voltage is 500mV, expected value is around 0x19A(410). But I get around 0x334(820). 

And input voltage is 1V, expected value is around 0x334(820). But I get around 0x668(1640). 

Working like 2.5V input range.

Also, there is one more problem.

If I get data more faster, peak point appears.

2 kHz data acquisition rate with around 500mV input.

10 kHz data acquisition rate with around 500mV input.

Here's logic analyzer capture (10kHz acquisition, input voltage around 500mV)

I did software reset before main loop.

I have no clue about this.

Parents Reply Children
  • This is my reset code.

    CONVST low time is 600ns. And after 1us, CS goes low.

    I checked VDD with oscilloscope. It's about 5.02v

  • Hi,  .

    VDD seems fine. CNVST low time also satisfies the condition of being pulled up before EOC. Can you share your schematic? What is your signal source? 


    On the other hand, I noticed on your timing diagram that you are using Mode 0 (CPOL=CPHA=0). Please ensure that your timing satisfies the condition of t12, the delay from the end of a conversion until the CS falling edge delay. And t10, the delay from CS falling edge until SDO exits the three-state condition. Lastly, the data is available from t2, data access time after SCLK falling edge.

    Warm regards,
    Jo

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.