Post Go back to editing

SNR Measurements in datasheet

Category: Datasheet/Specs
Product Number: AD7608

Hey,

Figure 19 in the datasheet for the AD7608 is showing results of signal to noise ratios that can be expected with different oversampling rates.

Is it possible to get any information on how this is measured?
I have the development board EVAL-AD7608SDZ, I assume that there has to be fitted a resistor shorting the pins of the SMB connector (R5 in schematic screenshot below).
If this is the case, do I short with 1Mohm resistor to match the input impedance of of the ADC, or to short it directly with 0 ohms.

Appended:

- Figure 19 from AD7068 datasheet
- Screenshot of V1 SMB connector from EVAL-AD7608SDZ schematics

Parents Reply Children
No Data