Post Go back to editing

Help Needed: Verifying AD7476A Sampling Rate with Zynq-Z2 and Jupyter

Category: Hardware
Product Number: AD7476A

Hi everyone,

Nice to meet you all! I am a university student studying in Korea and I am still a complete beginner. So, please don't look at my question too harshly and I would be extremely grateful for any advice or solutions you can provide.

Currently, I am using the Zynq-Z2 board and analyzing the AD7476A included in the Pmod AD1.

  1. I have confirmed from the datasheet that the AD7476A can achieve a maximum sampling rate of 1Msps with an SCLK of 20MHz. However, I want to verify this sampling rate in Jupyter. How can I do this?

  2. Is my understanding of the SCLK correct? Is it correct to divide the main frequency of the FPGA, which is 100MHz, down to 20MHz for use?

  3. For example, if I want to achieve a sampling rate of 100KHz instead of the maximum 1Msps and verify this in Jupyter with Python, what steps should I follow?

In short, I need a way to clearly confirm the sampling rate visually.

Thank you so much for your help!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.