In datasheet page 11 timing characteristics table 4.
t12(min)=3/MCLK at full power mode,
t12(min)=12/MCLK at mid power mode,
t12(min)=24/MCLK at low power mode,
does MCLK=614.4kHz or 2.4576MHz?
does MCLK vary at different power mode?
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
AD7124-8
Recommended for New Designs
The AD7124-8 is a low power, low noise, completely integrated
analog front end for high precision measurement applications. The
AD7124-8 W grade is AEC...
Datasheet
AD7124-8 on Analog.com
In datasheet page 11 timing characteristics table 4.
t12(min)=3/MCLK at full power mode,
t12(min)=12/MCLK at mid power mode,
t12(min)=24/MCLK at low power mode,
does MCLK=614.4kHz or 2.4576MHz?
does MCLK vary at different power mode?
Hi howardaaa ,
The AD7124-8 includes an internal 614.4 kHz clock on chip. This is the MCLK or Master Clock frequency equal to 614.4 kHz. However, this clock is internally divided, where the division factor being dependent on the power mode. Thus, the range of output data rates and performance is affected by the power mode.
You may also refer to the Table 52. Power Modes of the datasheet which also supports the page 11 timing characteristics table 4 you were referring to.
Thanks and regards,
Rod
Hi,
do you mean that at Mid Power, MCLK=153.6kHz?
But I think it's still 614.4k, because in the equation the numerator has changed from 3 to 12,
and 12/614.4k=3/153.6k.
Hi howardaaa ,
Apologies for the confusion. Yes, you are correct, the MCLK value to be used for the page 11 timing characteristics table 4 is 614.4kHz for the different power modes.
Regards,
Rod
Hi howardaaa ,
Apologies for the confusion. Yes, you are correct, the MCLK value to be used for the page 11 timing characteristics table 4 is 614.4kHz for the different power modes.
Regards,
Rod