CN0510 Use darlington transistor to enlarge output current to 50mA. If need output 350mA ,how to change the design base on CN0510?

AD5941
Recommended for New Designs
The AD5940 and AD5941 are high precision, low power analog front ends (AFEs) designed for portable applications that require high precision, electrochemical...
Datasheet
AD5941 on Analog.com
CN0510 Use darlington transistor to enlarge output current to 50mA. If need output 350mA ,how to change the design base on CN0510?

Hi,
Current through Darlington pair is controlled by below parameters in code:
pBATCfg->ACVoltPP = 300.0f; /* Pk-pk amplitude of excitation VBE */
pBATCfg->DCVolt = 1200.0f; /* Bias voltage of VBE*/
Transfer characteristic of this Darlington pair is shown in its datasheet:

Hi Akila,
1. I use Ltspice to simulation,change the V source does not change the output current significantly.But change the R3 from 62Ω to 2Ω, the vpp of output current will increase to about 400mA. Is there a problem with the simulation?
2. The AIN1 is just a monitor point?
3.pBATCfg->DCVolt = 1200.0f; /* Bias voltage of VBE*/
-> The max value is 2.4V?
4. pBATCfg->DCVolt = 1200.0f; /* Bias voltage of VBE*/
->The max value is 600mV?

Hi,
1. Your simulation output behavior is correct and as expected.
2. Yes. AIN1 is just a monitor point.
3. Yes. max of DC is 2.4V
4. Max of AC is 607mV
Hi Akila,
Thank you for your reply, but I still have some questions.
Simulation result as below figure1, DCVolt set 2.0V, ACVoltPP set 600mV, the VPP of output current just about 18mA, can't reach to 50mA .
if I need output 350mA , Is there only a way to reduce the value of R3(62Ω)?
figure1, output current 18mA

figure 2,output current 330mA

Hi,
Current through Darlington pair can be increased by increasing VBE and shown in graph. Maximum VBE is reached when R3 is 0 Ohms and DCVolt is set to max (2.4V).
Hi Akila,
Is there a formula for calculating input voltage and output current ?
The purpose of this circuit is convert Voltage to current , the same function can also be achieved using an OP-amp + mos ?
The formula about input voltage and output current is relatively simple.
Hi,
Yes. Purpose of this circuit is to convert ac voltage excitation to ac current excitation. Kindly refer to datasheet of Darlington pair for its transfer characteristics.
Hi,Akila
Thank you very much!
Hi,Akila
Refer to CN0510 schematic, the ADC of ad5491 support differential input ?
The volatage of battery or RCAL equal to (AIN3-AIN2)/441, how to set the input type of ADC?

Hi,Akila
Refer to CN0510 schematic, the ADC of ad5491 support differential input ?
The volatage of battery or RCAL equal to (AIN3-AIN2)/441, how to set the input type of ADC?

Hi,
AD5491's ADC supports differential input measurement.
In BatImpedance example code in github, ADC input is set by
dsp_cfg.ADCBaseCfg.ADCMuxN = ADCMUXN_AIN2;
dsp_cfg.ADCBaseCfg.ADCMuxP = ADCMUXP_AIN3;
Hi,
AD5491's ADC supports differential input measurement.
In BatImpedance example code in github, ADC input is set by
dsp_cfg.ADCBaseCfg.ADCMuxN = ADCMUXN_AIN2;
dsp_cfg.ADCBaseCfg.ADCMuxP = ADCMUXP_AIN3;
Hi,
Thank you for your reply!
Refer to schematic of CN0510, if PRExA or PRExB connect to LPF0, the value of AIN3 or AIN2 will equal to 0V. What is the purpose of this design?


Hi,
ADG1609 in schematic is used for precharging.
Hi,
Precharging is necessary?Why need precharging?
Before measure EIS , precharge AIN3 and AIN2 to zero?