Post Go back to editing

Internal or External reference

Category: Hardware
Product Number: MAX191

I was looking to verify the reference setup on a MAX191 we use. I read the datasheet and noted that a logic high input on the /PD line places the chip in in normal operation with an internal reference compensation mode. Currently, the device is powered with VDD as +5vdc and Vss is set to power supply return (0 vdc). The /PD pin is tied to +5vdc. So, I assume it is set for normal operation with an internal reference.

I also see in our schematic diagram that the VREF is also tied to +5vdc. as is REFADJ.  When you connect the REFADJ pin to VDD, it indicates that an external reference is to be used at VREF.

So, I am a little confused as to how this chip is functioning. Am I using an internal reference or an external reference?

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.