Post Go back to editing

ADAQ4001 Cant get the SPI communication to work

Category: Software
Product Number: ADAQ4001

Hello,

I am a beginner with the programming of microcontrollers and SPI communication and have some problems with the ADAQ4001 Evaluation Board.

I am planning to use the ADAQ on a custom board, but for a first test I am using the ADAQ Evaluation Board with a STM32 Nucelo Board.

The two Boards are connected with Jumper-Cables and therefore i have reduced the clock rate to roughly 300kHz.

For a first test I am just trying to read the Register of the ADAQ4001 and I am already running into problems.

I looked up the required timing from the Datasheet and it should look like this:

To check my software, i have a logic analyzer connected to the board.

The output waveform of my µC looks like this:

As far as i have understood the datasheet, the ADAQ should output the register values on the SDO line.

But for some reason there is no SDO Data from the ADAQ Board. The Pull-Up resistor for the SDO line is activated.

I have checked the power rails of the board and they look ok.

When i cycle the power to the ADAQ then there are sometimes random signals on the SDO line.

Can someone help me with the problem?

I am grateful for any tips.

Best regards,

Dennis

Edit Notes

Added Information
[edited by: DeBa at 5:34 AM (GMT -4) on 10 Apr 2024]
Parents
  • Hi  ,

    I'm assuming that you're operating on CS mode as the interface mode, since a single ADAQ4001 board is used. Please see the following suggestions:

    1. Add a CNV signal.
      1. This is significant because the CNV selects the interface mode of the device (see Datasheet pages 11 and 26).

    2. Change SDI default state to HIGH (I suggest modifying your CPOL and CPHA values in SPI configuration).
      1. CS mode should be selected instead (see page 10).
      2. Maybe your current setup selects Daisy-chain mode, and register reads are not allowed in this mode (see page 27).

    Let me know if this works. Thank you!

    Kind regards,
    Chelsea

  • Hello Chelsea,

    thank you very much for your answer.

    The solution was the missing CNV pulse before transmitting the config bits.

    The problem is now solved.

    Thanks and best regards,

    Dennis

Reply Children