Post Go back to editing

Need help with configuring AD5940

Thread Summary

The user was using the AD5940 BIA example to measure impedance with a 4-wire setup. They replaced capacitors with 0 Ohm resistors and got incorrect results. The solution involved reconfiguring the switch matrix settings: SWN_AIN1 to SWN_SE0, SWT_AIN1 to SWT_SE0LOAD, ADCMUXP_AIN3 to ADCMUXP_VRE0, and ADCMUXN_AIN2 to ADCMUXN_N_NODE. The user also encountered a frequency mismatch issue, which was resolved by restoring missing initialization lines in the code. The waveform now matches the set frequency and is stable.
AI Generated Content

Hello,

I'm using the AD5940 to measure impedances in a test circuit for now, i eventually want to use a 4 wire measurement so i can accurately measure this impedance. I'm using the BIA example on github since the Impedance example did not work for me. (https://github.com/analogdevicesinc/ad5940-examples/tree/master/examples/AD5940_BIA)

Right now my schematic looks like this and I've replaced the capacitors with 0 Ohm resistors. I get data but since I've not set up the matrix correctly I get wrong results (see image below). Can anyone help me to reconfigure the BIA example so it works for me?

Thanks

Thread Notes

Parents Reply Children