Post Go back to editing

Issue in output reading of ADAR7251

Category: Software

Hi,

     For ADAR7251, I have written the register value via SPI. The processor i used was BF548.  I want to read the output from ADAR7251. But i am not getting the output from ADAR7251. The following is the code i have written for reading.

PG2(Port G)--->CONV_START

PC4(Port C)--->DATA_READY

PC7(Port C)--->DATA_SCLK

PC8,PC9,PC10,PC11(Port C)---->DOUT

void Init_ADC_PORT(void)
{

int clk_len=15;

*pPORTG_FER = 0x0000;                                           // set PORTG to GPIO mode
*pPORTG_DIR_SET = PG2 | PG1;                              //Set as output pin
*pPORTG_INEN = 0x0000;                                          // enable as output
*pPORTG_CLEAR = 0x0000;
*pPORTG_MUX = 0x0000;


*pPORTC_FER = 0x0000;                                         // set PORTC to GPIO mode
*pPORTC_DIR_SET = PC4 | PC7 ;                          //Set as output pin
*pPORTC_INEN = PC8 | PC9 | PC10 | PC11 ;        // enable as input
 *pPORTC_CLEAR = 0x0000;
*pPORTC_MUX = 0x0000;

*pPORTG = *pPORTG | (1 << 2);                         // CONV_START=1

*pPORTC = *pPORTC & ~ (1 << 4);                     //DATA_READY=0

*pPORTG = *pPORTG & ~ (1 << 2);                     // CONV_START=0


*pPORTC = *pPORTC | (1 << 4);                         //DATA_READY=1

while(clk_len>=0)
{
*pPORTC = *pPORTC & ~ (1 << 7);                        //DATA_SCLK=0

*pPORTC = *pPORTC | (1 << 7);                             //DATA_SCLK=1

// printf("%u\t%u\t%u\t%u\n",(*pPORTC >> 8) & 1,(*pPORTC >> 9) & 1,(*pPORTC >> 10) & 1,(*pPORTC >> 11) & 1);


clk_len--;

}

*pPORTC = *pPORTC & ~ (1 << 7);                        //DATA_SCLK=0

}

when i check with the oscilloscope i am not able to read.

What may be the problem? 

Thanks.

Thread Notes

Top Replies

  • Hi  ,

    This part is not recommended for new designs and has unavailable technical support. You may want to consider using some of the newer parts which we have reference drivers and other collaterals…

Parents Reply Children
No Data