Hi.
I need to synchronize the acquisition of a MAX11261 ADC with other devices.
To achieve this, I generate a synchronization signal that I share between all devices.
In the case of the MAX11261, I have connected this synchronization signal to the SYNC pin and configured the device in sequencer mode 4 and set the value CRTL3:SYNC = 0 so that the device acts as a slave.
As far as I understand from the specifications, with this configuration, the delay value in DELAY:AUTOSCAN[7:0] should be ignored and the device should wakeup and start the scan on the transition from high to low on the SYNC pin, but this does not happen: the device adquires a data following the configuration of DELAY:AUTOSCAN value and ignore the SYNC pin.
Is there other considerations that I should take in account in order to synchronize a MAX11261 with other devices using the slave funciton?
Thanks in advance.