KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
AD5593R
Production
The AD5593R has eight input/output (I/O) pins, which can be
independently configured as digital-to-analog converter (DAC)
outputs, analog-to-digital converter...
Datasheet
AD5593R on Analog.com
I am trying to connect two AD5593R DACs to my raspberry pi which is running Kuiper Linux and when running iio_info command in terminal, it wouldn't detect any of them. At the first time running this I was able to detect one of them but upon disconnecting and connecting my HAT and DACs, it stopped detecting both of the DACs. Do you know what might have been the issue? could it be hardware related? I double checked all the connections and everything seem to be working fine. I also tried to attach one DAC at a time and still wouldn't detect.
I followed all the steps in the link below.
https://wiki.analog.com/resources/eval/user-guides/circuits-from-the-lab/eval-ad5593r-pmdz
this is the output I received running iio_info command:
analog@analog:/sys/bus/iio/devices/iio_sysfs_trigger $ sudo iio_info
[sudo] password for analog:
iio_info version: 0.25 (git tag:v0.25)
Libiio version: 0.25 (git tag: v0.25) backends: local xml ip usb serial
IIO context created with local backend.
Backend version: 0.25 (git tag: v0.25)
Backend description string: Linux analog 5.15.92-v7l+ #1 SMP Wed Dec 6 08:52:11 UTC 2023 armv7l
IIO context has 9 attributes:
hw_model: 0x0001 on Raspberry Pi 4 Model B Rev 1.5
hw_carrier: Raspberry Pi 4 Model B Rev 1.5
hw_mezzanine: 0x0001
hw_name: PMD-RPI-INTZ
hw_vendor: Analog Devices, Inc.
hw_serial: de4c9837-ed6a-41b2-a007-f26cc78cbdde
dtoverlay: rpi-ad5593r,vc4-kms-v3d
local,kernel: 5.15.92-v7l+
uri: local:
IIO context has 3 devices:
hwmon0: rpi_volt
1 channels found:
in0: (input)
1 channel-specific attributes found:
attr 0: lcrit_alarm value: 0
No trigger on this device
hwmon1: hidpp_battery_0
0 channels found:
No trigger on this device
iio_sysfs_trigger:
0 channels found:
2 device-specific attributes found:
attr 0: add_trigger ERROR: Permission denied (13)
attr 1: remove_trigger ERROR: Permission denied (13)
No trigger on this device
lallison - Moved from StudentZone (Analog Dialogue) to Precision ADCs. Post date updated from Thursday, March 14, 2024 1:50 AM UTC to Tuesday, June 24, 2025 9:21 PM UTC to reflect the move.
Hi BMSProject , I think I found the problem, assuming you're using the EVAL-AD5593r-PMDZ on the PMD-RPI-INTZ hat. The Pmod has a 100k pullup resistor on RESET, and these lines are tied to GPIO13 and GPIO17 on the Pmod connectors. These are set as inputs, but with weak internal pulldowns enabled, confirmed with:
sudo raspi-gpio get:
...
GPIO 13: level=0 fsel=0 func=INPUT pull=DOWN
...
GPIO 17: level=0 fsel=0 func=INPUT pull=DOWN
...
and indeed I measured the voltage at about 1.1V, which may have initially been read as high by the AD5593r, but then low (it's marginal.)
There are several ways to solve this, but adding:
gpio=13,17=pu,ip
to /boot/config.txt did the trick on my setup. I'll add this to the user guide.
-Mark
Hi Mark, thank you for your response. that indeed solved the issue but I still cannot detect both of the DACs at the same time. this is the output of terminal when running iio_info and it only detects one extra device instead of two when both of the DACs are connected:
analog@analog:~ $ iio_info iio_info version: 0.25 (git tag:v0.25) Libiio version: 0.25 (git tag: v0.25) backends: local xml ip usb serial IIO context created with local backend. Backend version: 0.25 (git tag: v0.25) Backend description string: Linux analog 5.15.92-v7l+ #1 SMP Wed Dec 6 08:52:11 UTC 2023 armv7l IIO context has 9 attributes: hw_model: 0x0001 on Raspberry Pi 4 Model B Rev 1.5 hw_carrier: Raspberry Pi 4 Model B Rev 1.5 hw_mezzanine: 0x0001 hw_name: PMD-RPI-INTZ hw_vendor: Analog Devices, Inc. hw_serial: de4c9837-ed6a-41b2-a007-f26cc78cbdde dtoverlay: rpi-ad5593r,vc4-kms-v3d local,kernel: 5.15.92-v7l+ uri: local: IIO context has 4 devices: hwmon0: rpi_volt 1 channels found: in0: (input) 1 channel-specific attributes found: attr 0: lcrit_alarm value: 0 No trigger on this device hwmon1: hidpp_battery_0 0 channels found: No trigger on this device iio:device0: ad5593r 5 channels found: voltage2: (output) 3 channel-specific attributes found: attr 0: raw value: 0 attr 1: scale value: 0.610351562 attr 2: scale_available value: 0.610351562 1.220703124 voltage1: (input) 3 channel-specific attributes found: attr 0: raw value: 37 attr 1: scale value: 0.610351562 attr 2: scale_available value: 0.610351562 1.220703124 voltage0: (output) 3 channel-specific attributes found: attr 0: raw value: 0 attr 1: scale value: 0.610351562 attr 2: scale_available value: 0.610351562 1.220703124 voltage2: (input) 3 channel-specific attributes found: attr 0: raw value: 1 attr 1: scale value: 0.610351562 attr 2: scale_available value: 0.610351562 1.220703124 temp: (input) 3 channel-specific attributes found: attr 0: offset value: -753 attr 1: raw value: 831 attr 2: scale value: 376.789750000 No trigger on this device iio_sysfs_trigger: 0 channels found: 2 device-specific attributes found: attr 0: add_trigger ERROR: Permission denied (13) attr 1: remove_trigger ERROR: Permission denied (13) No trigger on this device
one more question. I am trying to use these DACs to get voltage levels of 0.1V to 1.6V to feed to my circuit. Do you know if I can do this using PyADDI-IIO?
Hi BMSProject , sorry for the delay. Have you set the two devices to two different addresses? You will also need to enable two instances of the device tree overlay, one with"
,addr=0x11
appended.
If you don't see the two devices after that, you can scan the I2C bus with:
i2cdetect -y 1
You should see a number for a device that does not have a driver bound to it, and "UU" for those that do.
-Mark