Hi!
I'm working with the MAX31865. I built a prototype with the recommended circuit shown in the datasheet for 3-wires and I can communicate wit the IC ok.
The matter is that it is measuring with a big error, like a 15%. The error is either obtain with a PT100 or if I connect a fixed 100 ohm resistor.
For example, in the case of the 100 ohm resistor, it measures 115 ohm. The reference resistor is a high-precision 400 ohm.
Can anyone help me?
Thanks!