Post Go back to editing

DC718C

Category: Datasheet/Specs
Product Number: DC718C

Hello, 

Im currently working with the DC718C data collection board, and i'm using P-Scope to collect the data and MATLAB for further processing. I want to know if its possible to collect more than 131072 samples (Which is the maximum amount of samples i can extract from P-Scope), by either using P-Scope or another alternative? The datasheet says. " The Linear Technology supplied PScope evaluation software automatically detects the DC718 and in select cases can also detect the ADC demonstration circuit under evaluation. This system provides for fast and easy performance evaluation of high speed ADCs by collecting up to 128k word samples". So i want to know if the limitation is due to the memory data buffer or simply the P-Scope software. 

Thread Notes

Parents Reply
  • Thank you for your response. I'm wondering if there are any YouTube tutorials available that demonstrate the process of data collection using MATLAB? I've encountered some challenges with linear lab tools, and I believe visual guidance could be beneficial. Additionally, I'm considering purchasing a new data collection board compatible with LTC238-18. Could you kindly recommend a board capable of capturing approximately 1 million samples? 

Children
No Data