Post Go back to editing

MAX22531 external usage of VREF

Thread Summary

The user is experiencing issues with resistance measurements using the MAX22531, where ADC readings do not match oscilloscope measurements when VREF is externally connected to ground or AIN1 through switches. The final answer directs the user to visit Analog Devices' technical support pages for further assistance, without addressing the specific issue of using VREF externally.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX22531

Hi, we are using a MAX22531 to conduct a resistance measurement.

We use the VREF pin externally to have an accurate reference voltage. The circuit looks something like this:

So we use switch SW1 to either connect VREF to ground with R1 or to AIN1 with R2.

We are seeing issues with this setup and the voltages read from the ADC do not correspond with what we see on the oscilloscope. VREF seemed stable at 1.8V.

In the datasheet I did not find anything about using the VREF pin externally and pulling (very little) current. Is that OK, or is the pin only for capacitors to stabilize the internal reference?

Edit Notes

Added LMXMprodsupport to tags
[edited by: JEstayo at 12:11 PM (GMT -5) on 5 Mar 2024]