What is the input impedance (or drive requirements) for the COM input? Can I connect this to Vref/2 in order to get full range on my single ended inputs? If I ground COM and REF- then my single ended inputs have a full scale value of only Vref/2.
LTC2495
Production
The LTC2495 is a 16-channel (eight differential), 16-bit, No Latency ΔΣ™ ADC with Easy Drive technology and a 2-wire, I2C interface. The patented...
Datasheet
LTC2495 on Analog.com
What is the input impedance (or drive requirements) for the COM input? Can I connect this to Vref/2 in order to get full range on my single ended inputs? If I ground COM and REF- then my single ended inputs have a full scale value of only Vref/2.
JEstayo - Moved from Precision ADCs to Amplifiers. Post date updated from Sunday, March 3, 2024 7:29 PM UTC to Monday, March 4, 2024 1:55 AM UTC to reflect the move.
GLADION - Moved from Amplifiers to Precision ADCs. Post date updated from Monday, March 4, 2024 1:55 AM UTC to Monday, March 4, 2024 2:56 AM UTC to reflect the move.
Hello gjleeson ,
The COM input impedance is the same as other analog inputs, as these "see" the same ADC input through the multiplexer. You certainly can connect a mid-supply VREF through COM, just make sure that the source impedance will be lower than 10k ohms to ensure proper settling.
If you are experiencing accuracy issues due to input voltage not settling right, you may use an external buffer as shown below.

Regards,
Yugel