Hello,
We are using the AD7980 in the 3-wire mode without busy indicator where we have SDI tied to VIO (3v3), in our operation we turn on the VDD (2v5) before we turn on the VIO, and REF is at 5V. When we power VDD before VIO, during the period before VDD is turned on, we see square waves being sent out from the VDD pin causing an immense amount of noise in the system, are these square waves potentially from the SDI pin? If yes, what is the best way to eliminate this issue? Our power-up sequence is VDD (2v5), VIO (3v3) next, and REF (5v) last.
If I understand the datasheet correctly, the "When VIO is greater than or equal to VDD, the AD7980 is insensitive to power supply sequencing" statement, made us not consider the power sequence. Is there something we should be carful about?
Thank you for your help in advance!