Post Go back to editing

ADAS1000 ECG and Impedance

Category: Software
Product Number: ADAS1000

Hi,
The requirement is to measure the ECG signal using two chest electrodes by ADAS1000. Also to measure the Thoracic impedance measurement which is mentioned in the datasheet. What are all the possible ways it could be done. I went through the examples of ADAS1000 datasheet but still need clarity in both hardware connections and software settings.

What is the input and what is the respiration internal and external path? 

Is ADAS1000 is good for obtaining trans thoracic impedance? else what is used to obtain it?

I have ADAS1000SDZ EVAL board and dsPIC33EP / STM32 controllers.