Post Go back to editing

AD7699

Category: Datasheet/Specs
Product Number: AD7689

Hello,

I plan to use the AD7699 and I need to clarify how the configuration register initialization work after power-up.

The datasheet states:

"Note that at power-up, the CFG register is undefined and two dummy conversions are required to update the register" on page 24.

and

"the first 14 SCK rising edges update the CFG" on page 27.

So if I send the sequence "Conversion pulse + an SPI frame with only 14 SCK periods" twice.

Is the configuration register updated ?

Is the configuration register updated on the 14th SCK rising edge ? If not, what is the internal event updating CFG reg ?  

I plan to use the ADC in the mode Read/write after convert with a busy indicator.

Thanks for your help,

Regards,

Stéphane