Post Go back to editing

AD7173-8: ADC not working with input buffers enabled

Category: Hardware
Product Number: AD7173-8

Whenever I enable either the analog input buffers or the reference input buffers for the ADC, we read a value of -8385495 (-27.5V) when 0V is applied differentially and -2294797 (-7.5V) when 10V is applied. This only happens on certain ADCs (we have 4 on our board), and it is a different ADC on each board so I don't think it's a schematic/layout issue. Our power supply is slightly noisy, could this cause any issues? We measured a peak to peak ripple between each supply and ground of 260 mV on the +2.5V supply, 260 mV on the +3.3V supply, and 332 mV on the -2.5V supply.

I also read back the value of the setup configuration register to make sure the buffer enable [1:0] bits were being set correctly for both the reference buffers and the analog input buffers.

Edit Notes

Added product number on subject
[edited by: JCCillion at 12:17 AM (GMT -5) on 14 Feb 2024]
Parents Reply Children