Post Go back to editing

AD7606C-16 || Digital Data to Voltage Conversion

Category: Hardware
Product Number: AD7606C-16

Hi Team,

I am using AD7606C-16 ADC IC for my receiver system.  I want to validate the ADC-received samples to my scope waveform. I am doubting what should I consider the value of Full Scale Range in the calculation formula.

Please Note: I haven't made any configuration changes for the ADC IC. 

Conversion formula:

Voltage= (Digital Data)* Full Scale Range / ((2^16)-1)

In the Oscilloscope I am seeing Vpp (measured at P wrt N I/p of ADC) is ~3.0Vpp

I am attaching the Digital Data, Pls suggest are the samples Ok. What Should I consider the Full Scale Range for my calculation?
CONVST Freq: 108KHz
Input Frequency: 27KHz


Parents
  • -2379	-2477	-2362	-2390	-2293	-2437	-2502	-2305	-2276	-2333	-2269	-2405	-2356	-2282	-2349	-2419	-2432	-2405	-2366	-2404	-2412	-2330	-2339	-2555	-2477	-2248	-2549	-2455	-2408	-2491	-2362	-2430
    2730	2717	2565	2874	2654	2783	2821	2700	2703	2810	2827	2923	2657	2637	2666	2698	2807	3017	2583	2662	2482	2776	2799	2541	2587	2734	2603	2641	2818	2810	2705	2834
    2148	2201	2121	2149	2003	2192	2242	2071	2020	2059	1992	2133	2095	2039	2110	2230	2243	2217	2056	2175	2095	2065	2075	2288	2278	2050	2320	2204	2201	2294	2234	2258
    -2966	-2996	-2810	-3117	-2948	-3033	-3079	-2937	-2959	-3094	-3108	-3201	-2920	-2886	-2908	-2892	-3002	-3206	-2895	-2894	-2803	-3041	-3069	-2814	-2794	-2935	-2839	-2897	-3031	-3014	-2840	-3011
    -2386	-2477	-2371	-2392	-2298	-2441	-2501	-2308	-2278	-2341	-2273	-2411	-2360	-2289	-2356	-2426	-2439	-2404	-2367	-2407	-2418	-2327	-2342	-2558	-2482	-2250	-2553	-2453	-2412	-2495	-2369	-2435
    2735	2718	2566	2875	2659	2785	2820	2702	2705	2819	2834	2924	2658	2637	2668	2699	2808	3018	2583	2662	2485	2773	2807	2543	2596	2734	2608	2644	2824	2809	2709	2836
    2154	2201	2130	2153	2008	2196	2241	2077	2024	2066	1999	2138	2100	2046	2119	2238	2247	2220	2056	2181	2101	2065	2076	2293	2281	2055	2322	2203	2204	2299	2238	2264
    -2967	-2995	-2809	-3116	-2953	-3031	-3073	-2938	-2960	-3100	-3111	-3200	-2918	-2884	-2908	-2893	-3000	-3208	-2890	-2894	-2804	-3036	-3072	-2817	-2796	-2935	-2839	-2898	-3032	-3014	-2839	-3014
    -2393	-2476	-2378	-2396	-2303	-2445	-2503	-2313	-2284	-2346	-2280	-2417	-2366	-2295	-2362	-2431	-2439	-2409	-2366	-2414	-2422	-2332	-2343	-2564	-2482	-2257	-2556	-2455	-2416	-2501	-2369	-2443
    2732	2716	2565	2875	2665	2781	2813	2702	2706	2820	2835	2922	2657	2635	2667	2699	2810	3019	2579	2661	2487	2771	2810	2545	2597	2734	2607	2645	2823	2812	2707	2837
    2159	2201	2133	2159	2010	2202	2244	2079	2029	2071	2002	2142	2107	2048	2121	2238	2246	2223	2056	2186	2103	2069	2077	2293	2283	2060	2326	2202	2209	2300	2238	2268
    -2966	-2988	-2811	-3117	-2959	-3027	-3072	-2938	-2963	-3100	-3113	-3198	-2918	-2883	-2906	-2890	-3005	-3206	-2887	-2889	-2810	-3032	-3074	-2813	-2797	-2934	-2838	-2896	-3034	-3014	-2838	-3014
    -2395	-2475	-2381	-2400	-2307	-2450	-2508	-2314	-2289	-2348	-2285	-2419	-2373	-2293	-2364	-2430	-2437	-2414	-2367	-2418	-2425	-2335	-2343	-2565	-2487	-2262	-2560	-2456	-2420	-2502	-2369	-2444
    2729	2710	2565	2877	2667	2780	2810	2702	2710	2821	2833	2919	2653	2635	2663	2695	2811	3020	2574	2659	2490	2767	2807	2541	2594	2733	2606	2642	2822	2813	2702	2836
    2159	2204	2135	2161	2014	2206	2250	2081	2033	2071	2006	2144	2114	2044	2121	2236	2244	2228	2057	2188	2104	2072	2077	2292	2286	2064	2329	2203	2210	2300	2235	2267
    -2963	-2983	-2809	-3117	-2959	-3026	-3070	-2936	-2967	-3099	-3109	-3193	-2916	-2884	-2900	-2887	-3003	-3209	-2883	-2891	-2810	-3032	-3070	-2808	-2794	-2932	-2836	-2893	-3033	-3012	-2830	-3007
    -2394	-2482	-2381	-2402	-2309	-2456	-2511	-2316	-2290	-2350	-2285	-2420	-2378	-2292	-2362	-2426	-2436	-2416	-2370	-2416	-2426	-2336	-2345	-2562	-2490	-2263	-2563	-2456	-2422	-2499	-2367	-2441
    2724	2704	2563	2874	2665	2776	2812	2698	2713	2817	2829	2914	2656	2636	2656	2687	2812	3020	2571	2658	2490	2765	2804	2533	2590	2729	2605	2637	2823	2807	2694	2824
    2157	2208	2137	2160	2015	2211	2251	2082	2035	2072	2004	2146	2117	2044	2120	2232	2243	2228	2061	2183	2107	2073	2082	2292	2290	2064	2332	2204	2213	2297	2236	2269
    -2956	-2981	-2805	-3113	-2955	-3023	-3070	-2931	-2967	-3095	-3103	-3190	-2918	-2884	-2894	-2878	-3003	-3211	-2881	-2888	-2808	-3029	-3064	-2801	-2789	-2929	-2835	-2890	-3031	-3006	-2822	-2997
    -2393	-2486	-2382	-2399	-2311	-2457	-2509	-2316	-2291	-2347	-2282	-2421	-2379	-2292	-2361	-2422	-2435	-2414	-2372	-2412	-2427	-2337	-2348	-2563	-2491	-2264	-2562	-2456	-2423	-2498	-2367	-2446
    2717	2708	2557	2868	2657	2775	2809	2693	2711	2812	2821	2912	2654	2635	2649	2682	2806	3022	2570	2654	2485	2765	2796	2528	2586	2727	2603	2636	2821	2801	2688	2817
    2158	2212	2136	2161	2014	2210	2244	2083	2033	2067	2002	2145	2113	2045	2119	2230	2242	2225	2062	2178	2109	2072	2083	2292	2291	2063	2328	2204	2212	2294	2235	2270
    -2950	-2984	-2798	-3105	-2945	-3022	-3065	-2927	-2964	-3086	-3097	-3189	-2917	-2881	-2887	-2872	-2994	-3206	-2880	-2881	-2802	-3026	-3057	-2796	-2785	-2925	-2836	-2887	-3029	-2997	-2818	-2989
    -2393	-2487	-2380	-2400	-2306	-2452	-2500	-2315	-2288	-2341	-2278	-2415	-2372	-2293	-2360	-2421	-2437	-2408	-2372	-2404	-2428	-2331	-2347	-2557	-2490	-2259	-2555	-2453	-2420	-2490	-2368	-2442
    2713	2710	2552	2863	2649	2776	2802	2690	2707	2804	2817	2912	2652	2633	2644	2678	2799	3014	2568	2647	2478	2762	2789	2524	2582	2724	2602	2634	2816	2793	2686	2811
    2155	2208	2132	2158	2009	2198	2236	2077	2030	2061	1995	2134	2104	2045	2115	2227	2241	2220	2056	2173	2107	2066	2080	2286	2286	2058	2317	2200	2205	2288	2233	2266
    -2947	-2988	-2795	-3101	-2939	-3022	-3060	-2925	-2959	-3082	-3095	-3188	-2912	-2881	-2887	-2872	-2987	-3200	-2878	-2877	-2796	-3026	-3050	-2795	-2782	-2926	-2831	-2888	-3022	-2994	-2819	-2988
    -2388	-2478	-2375	-2395	-2300	-2437	-2492	-2307	-2285	-2335	-2268	-2402	-2361	-2289	-2355	-2416	-2433	-2406	-2363	-2401	-2427	-2325	-2342	-2551	-2487	-2255	-2544	-2451	-2412	-2486	-2363	-2437
    2714	2713	2552	2862	2646	2776	2803	2692	2706	2804	2822	2914	2652	2635	2650	2681	2798	3011	2570	2647	2479	2763	2789	2526	2587	2728	2602	2638	2814	2795	2691	2815
    2151	2199	2127	2152	2004	2186	2230	2072	2026	2055	1985	2123	2094	2039	2110	2221	2240	2217	2049	2171	2106	2059	2073	2278	2283	2052	2311	2197	2200	2281	2230	2258
    -2951	-2991	-2801	-3105	-2944	-3026	-3066	-2931	-2963	-3087	-3104	-3193	-2917	-2886	-2897	-2879	-2994	-3200	-2884	-2882	-2803	-3031	-3058	-2799	-2793	-2934	-2836	-2897	-3023	-3003	-2827	-2996
    -2388	-2470	-2371	-2390	-2297	-2431	-2492	-2302	-2281	-2330	-2262	-2394	-2356	-2285	-2352	-2413	-2434	-2407	-2358	-2402	-2426	-2323	-2337	-2550	-2484	-2252	-2543	-2449	-2410	-2480	-2360	-2433
    2720	2716	2560	2866	2656	2783	2812	2698	2710	2811	2829	2921	2656	2641	2660	2691	2805	3015	2574	2657	2485	2769	2798	2532	2594	2738	2605	2648	2814	2806	2699	2827
    2154	2196	2126	2153	2003	2186	2234	2068	2023	2052	1982	2122	2093	2038	2110	2222	2241	2222	2046	2174	2108	2063	2070	2283	2283	2052	2313	2198	2201	2278	2229	2259
    -2958	-2993	-2808	-3109	-2953	-3034	-3077	-2936	-2967	-3095	-3109	-3198	-2921	-2892	-2906	-2888	-3003	-3207	-2890	-2892	-2811	-3038	-3069	-2806	-2799	-2942	-2843	-2905	-3028	-3011	-2834	-3009
    -2395	-2474	-2372	-2395	-2299	-2438	-2499	-2305	-2281	-2334	-2263	-2403	-2358	-2286	-2353	-2417	-2437	-2412	-2360	-2406	-2432	-2330	-2338	-2556	-2489	-2253	-2550	-2451	-2416	-2480	-2364	-2435
    2725	2717	2567	2870	2664	2791	2820	2702	2713	2819	2835	2927	2660	2645	2667	2698	2813	3020	2581	2664	2495	2778	2809	2536	2599	2742	2614	2652	2820	2808	2704	2835
    2160	2202	2129	2161	2007	2195	2243	2073	2025	2058	1988	2135	2097	2041	2112	2229	2247	2226	2051	2179	2114	2072	2074	2291	2290	2055	2322	2202	2209	2285	2235	2264
    -2962	-2994	-2812	-3111	-2961	-3040	-3081	-2938	-2970	-3102	-3115	-3205	-2922	-2892	-2910	-2893	-3007	-3215	-2892	-2898	-2818	-3047	-3077	-2811	-2800	-2943	-2847	-2906	-3033	-3013	-2835	-3014
    -2400	-2478	-2378	-2404	-2302	-2445	-2508	-2310	-2283	-2337	-2269	-2413	-2363	-2290	-2357	-2422	-2440	-2416	-2363	-2413	-2434	-2341	-2342	-2564	-2494	-2256	-2555	-2457	-2422	-2494	-2369	-2442
    2727	2718	2567	2871	2668	2794	2820	2704	2712	2824	2837	2930	2660	2642	2667	2700	2815	3028	2580	2669	2500	2785	2814	2541	2596	2743	2615	2652	2826	2812	2703	2838
    2164	2208	2133	2169	2007	2203	2250	2081	2026	2061	1992	2142	2102	2046	2115	2233	2247	2227	2055	2184	2113	2080	2076	2296	2295	2057	2326	2207	2212	2297	2241	2270
    -2961	-2995	-2812	-3110	-2962	-3041	-3080	-2939	-2967	-3102	-3115	-3205	-2923	-2887	-2907	-2893	-3006	-3215	-2888	-2898	-2822	-3049	-3081	-2810	-2794	-2941	-2846	-2899	-3036	-3015	-2834	-3012
    -2399	-2482	-2380	-2410	-2300	-2451	-2514	-2316	-2284	-2338	-2271	-2421	-2365	-2295	-2356	-2427	-2439	-2412	-2369	-2413	-2430	-2343	-2343	-2566	-2497	-2256	-2559	-2462	-2423	-2499	-2375	-2445
    2725	2718	2565	2873	2667	2792	2818	2706	2709	2822	2834	2930	2659	2637	2662	2700	2810	3028	2576	2669	2500	2787	2813	2540	2588	2739	2611	2645	2825	2816	2700	2837
    2161	2206	2133	2171	2003	2206	2252	2082	2027	2061	1994	2145	2101	2051	2111	2234	2243	2223	2058	2185	2106	2082	2075	2300	2296	2057	2324	2215	2209	2301	2244	2272
    -2959	-2994	-2810	-3112	-2959	-3036	-3077	-2940	-2964	-3096	-3110	-3204	-2922	-2884	-2903	-2893	-3000	-3214	-2884	-2897	-2814	-3048	-3077	-2810	-2785	-2937	-2838	-2895	-3031	-3017	-2828	-3012
    -2397	-2478	-2379	-2409	-2294	-2451	-2512	-2313	-2284	-2337	-2274	-2420	-2363	-2296	-2353	-2424	-2438	-2408	-2372	-2413	-2422	-2344	-2342	-2571	-2500	-2256	-2558	-2469	-2420	-2500	-2377	-2446
    2722	2716	2562	2873	2663	2784	2814	2705	2706	2815	2829	2930	2656	2636	2661	2699	2806	3023	2574	2666	2490	2783	2810	2540	2586	2735	2607	2641	2818	2814	2697	2836
    2160	2202	2132	2170	1998	2206	2247	2079	2024	2061	1996	2144	2097	2051	2110	2232	2246	2220	2061	2181	2103	2079	2077	2299	2298	2055	2326	2219	2211	2297	2245	2270
    -2956	-2988	-2805	-3111	-2954	-3027	-3071	-2937	-2961	-3091	-3106	-3206	-2916	-2883	-2903	-2891	-2998	-3210	-2886	-2893	-2806	-3043	-3074	-2811	-2787	-2934	-2838	-2896	-3025	-3013	-2827	-3008
    -2396	-2476	-2379	-2410	-2293	-2455	-2506	-2313	-2279	-2339	-2278	-2417	-2360	-2297	-2351	-2423	-2442	-2407	-2372	-2411	-2422	-2343	-2343	-2570	-2497	-2256	-2560	-2472	-2421	-2498	-2375	-2445
    2720	2711	2557	2869	2659	2778	2808	2701	2703	2811	2827	2930	2650	2637	2661	2695	2805	3020	2575	2661	2480	2776	2803	2540	2587	2732	2602	2643	2811	2809	2692	2832
    2158	2203	2133	2169	2000	2210	2244	2079	2021	2064	2000	2142	2099	2051	2109	2232	2251	2219	2060	2179	2103	2079	2080	2297	2292	2056	2327	2217	2211	2296	2241	2269
    -2951	-2985	-2800	-3106	-2952	-3022	-3064	-2934	-2957	-3088	-3104	-3203	-2910	-2884	-2903	-2886	-2999	-3207	-2886	-2886	-2798	-3034	-3068	-2809	-2789	-2931	-2833	-2895	-3022	-3006	-2823	-3002
    -2395	-2478	-2379	-2409	-2297	-2453	-2504	-2312	-2276	-2341	-2282	-2413	-2364	-2296	-2351	-2422	-2447	-2405	-2372	-2407	-2425	-2341	-2347	-2564	-2492	-2255	-2559	-2463	-2421	-2495	-2371	-2443
    2714	2707	2552	2865	2659	2776	2803	2695	2700	2809	2825	2923	2645	2636	2659	2691	2807	3016	2576	2652	2476	2767	2800	2536	2586	2727	2600	2641	2810	2802	2690	2824
    2157	2205	2132	2170	2003	2205	2243	2078	2016	2065	2001	2136	2100	2049	2109	2231	2252	2219	2059	2178	2107	2079	2082	2292	2289	2055	2325	2209	2210	2295	2236	2269
    -2947	-2979	-2797	-3102	-2952	-3021	-3064	-2927	-2957	-3087	-3105	-3194	-2906	-2882	-2899	-2882	-2999	-3202	-2886	-2879	-2795	-3028	-3062	-2806	-2786	-2927	-2830	-2892	-3020	-3004	-2820	-2999
    -2392	-2478	-2376	-2408	-2297	-2448	-2503	-2310	-2270	-2341	-2282	-2408	-2364	-2293	-2355	-2423	-2444	-2406	-2371	-2410	-2425	-2341	-2347	-2561	-2486	-2255	-2556	-2456	-2418	-2495	-2366	-2445
    2710	2705	2549	2862	2658	2774	2803	2691	2699	2810	2826	2915	2643	2636	2658	2689	2808	3013	2576	2647	2477	2763	2798	2534	2584	2726	2600	2636	2811	2804	2689	2823
    2155	2204	2127	2167	2002	2198	2242	2075	2013	2062	2000	2132	2100	2045	2112	2227	2248	2217	2058	2181	2104	2078	2080	2289	2284	2053	2321	2200	2206	2292	2231	2266
    -2948	-2982	-2798	-3102	-2952	-3021	-3065	-2926	-2959	-3091	-3105	-3187	-2910	-2882	-2902	-2884	-2999	-3197	-2886	-2874	-2799	-3025	-3065	-2802	-2784	-2925	-2833	-2885	-3024	-3006	-2821	-2997
    -2390	-2478	-2368	-2404	-2292	-2442	-2500	-2308	-2267	-2337	-2276	-2404	-2361	-2288	-2356	-2416	-2438	-2403	-2367	-2409	-2422	-2339	-2344	-2557	-2483	-2250	-2550	-2450	-2414	-2488	-2362	-2437
    2714	2710	2555	2862	2660	2775	2808	2693	2707	2815	2827	2912	2651	2635	2661	2694	2805	3012	2572	2649	2480	2766	2799	2535	2583	2727	2602	2634	2813	2809	2691	2825
    2154	2203	2118	2164	1996	2196	2238	2075	2010	2059	1996	2130	2097	2040	2113	2224	2241	2216	2054	2180	2099	2077	2077	2289	2280	2050	2315	2200	2201	2286	2229	2262
    -2952	-2989	-2804	-3103	-2952	-3024	-3070	-2930	-2969	-3096	-3108	-3190	-2918	-2884	-2906	-2890	-2997	-3200	-2886	-2883	-2804	-3033	-3068	-2807	-2787	-2931	-2838	-2890	-3026	-3015	-2827	-3003
    -2390	-2478	-2363	-2401	-2290	-2442	-2501	-2311	-2268	-2332	-2275	-2403	-2360	-2285	-2357	-2413	-2435	-2404	-2367	-2409	-2421	-2340	-2343	-2561	-2484	-2251	-2548	-2451	-2413	-2487	-2362	-2435
    2717	2716	2560	2863	2658	2780	2811	2700	2714	2817	2830	2918	2656	2639	2665	2701	2806	3013	2574	2657	2486	2773	2802	2536	2587	2733	2609	2639	2817	2816	2698	2830
    2156	2204	2118	2160	1996	2197	2243	2078	2014	2055	1998	2132	2101	2042	2115	2222	2244	2219	2057	2182	2102	2078	2078	2293	2285	2052	2319	2201	2206	2287	2234	2262
    -2955	-2993	-2808	-3102	-2955	-3027	-3074	-2936	-2977	-3094	-3111	-3196	-2921	-2886	-2910	-2896	-2997	-3204	-2888	-2893	-2808	-3042	-3069	-2810	-2790	-2937	-2844	-2895	-3030	-3021	-2834	-3010
    -2392	-2483	-2367	-2403	-2291	-2445	-2505	-2314	-2274	-2334	-2276	-2410	-2367	-2291	-2360	-2415	-2439	-2408	-2368	-2416	-2424	-2342	-2345	-2569	-2488	-2254	-2554	-2456	-2419	-2492	-2369	-2438
    2721	2720	2561	2861	2661	2782	2812	2704	2724	2813	2832	2924	2657	2641	2666	2702	2800	3020	2574	2666	2487	2779	2802	2542	2588	2740	2609	2644	2817	2821	2704	2837
    2159	2211	2126	2163	2000	2200	2248	2080	2019	2057	1997	2138	2110	2049	2121	2224	2248	2222	2058	2188	2108	2080	2082	2300	2291	2057	2327	2205	2212	2295	2241	2266
    -2956	-2996	-2808	-3100	-2955	-3030	-3073	-2938	-2980	-3088	-3110	-3201	-2920	-2887	-2906	-2891	-2995	-3211	-2886	-2898	-2808	-3040	-3066	-2810	-2788	-2939	-2842	-2892	-3029	-3020	-2840	-3009
    -2396	-2490	-2374	-2406	-2296	-2449	-2511	-2314	-2278	-2339	-2277	-2415	-2376	-2299	-2366	-2420	-2446	-2408	-2371	-2418	-2430	-2343	-2348	-2569	-2495	-2258	-2562	-2457	-2426	-2498	-2375	-2440
    2718	2720	2561	2860	2658	2782	2810	2703	2721	2808	2828	2928	2655	2640	2659	2694	2802	3025	2572	2667	2487	2771	2796	2539	2586	2739	2609	2640	2816	2818	2707	2833
    2161	2215	2132	2169	2002	2203	2252	2079	2022	2065	1997	2140	2116	2054	2125	2231	2255	2221	2058	2190	2113	2082	2083	2300	2298	2062	2331	2208	2216	2301	2244	2267
    -2951	-2991	-2808	-3100	-2950	-3025	-3069	-2932	-2974	-3083	-3102	-3200	-2918	-2884	-2899	-2879	-2992	-3212	-2880	-2896	-2805	-3030	-3059	-2807	-2785	-2937	-2838	-2891	-3025	-3018	-2839	-3003
    -2395	-2490	-2376	-2407	-2294	-2451	-2512	-2313	-2278	-2344	-2274	-2415	-2380	-2300	-2364	-2426	-2448	-2407	-2369	-2420	-2435	-2346	-2348	-2567	-2499	-2260	-2565	-2461	-2425	-2503	-2374	-2444
    2712	2716	2563	2864	2653	2779	2808	2696	2714	2806	2820	2926	2654	2639	2653	2684	2799	3020	2570	2663	2484	2761	2792	2535	2583	2734	2605	2638	2814	2812	2706	2824
    2160	2212	2129	2164	1999	2202	2251	2075	2022	2066	1997	2139	2115	2050	2121	2236	2253	2219	2056	2188	2113	2081	2082	2294	2298	2057	2330	2207	2212	2301	2241	2267
    -2948	-2989	-2808	-3107	-2946	-3024	-3068	-2926	-2969	-3085	-3099	-3200	-2919	-2883	-2895	-2874	-2993	-3201	-2881	-2891	-2802	-3019	-3057	-2801	-2786	-2932	-2836	-2889	-3026	-3008	-2836	-2993
    -2392	-2484	-2370	-2400	-2289	-2448	-2509	-2307	-2278	-2343	-2274	-2412	-2374	-2294	-2358	-2429	-2443	-2407	-2365	-2416	-2431	-2345	-2345	-2562	-2497	-2256	-2557	-2459	-2419	-2502	-2370	-2442
    2710	2712	2563	2873	2651	2779	2807	2689	2710	2809	2821	2926	2655	2637	2654	2684	2801	3015	2569	2661	2481	2756	2791	2532	2583	2733	2602	2641	2814	2806	2701	2818
    2156	2206	2122	2156	1994	2198	2247	2072	2020	2064	1996	2135	2107	2045	2111	2235	2244	2220	2051	2183	2108	2080	2080	2289	2293	2054	2318	2205	2204	2299	2234	2266
    -2946	-2983	-2808	-3112	-2946	-3022	-3068	-2919	-2965	-3085	-3102	-3200	-2921	-2882	-2898	-2877	-2995	-3199	-2882	-2891	-2802	-3022	-3063	-2802	-2788	-2934	-2833	-2895	-3029	-3007	-2833	-2993
    -2388	-2478	-2365	-2394	-2288	-2442	-2505	-2305	-2275	-2339	-2276	-2408	-2365	-2290	-2349	-2427	-2434	-2408	-2363	-2412	-2426	-2342	-2344	-2558	-2495	-2251	-2546	-2454	-2413	-2499	-2365	-2439
    2710	2710	2561	2875	2654	2778	2806	2685	2705	2809	2823	2930	2657	2636	2655	2688	2801	3011	2571	2660	2481	2759	2801	2531	2589	2734	2600	2643	2820	2805	2702	2820
    2153	2202	2122	2154	1996	2194	2245	2070	2019	2059	1998	2131	2099	2043	2105	2232	2238	2224	2054	2182	2106	2077	2078	2289	2292	2055	2312	2201	2200	2297	2232	2264
    -2949	-2981	-2807	-3113	-2950	-3024	-3068	-2920	-2962	-3084	-3105	-3204	-2922	-2882	-2898	-2883	-2995	-3198	-2882	-2891	-2803	-3025	-3070	-2802	-2793	-2934	-2832	-2896	-3032	-3008	-2833	-2998
    -2387	-2479	-2368	-2395	-2291	-2441	-2505	-2306	-2274	-2336	-2277	-2404	-2360	-2289	-2346	-2421	-2430	-2412	-2366	-2411	-2423	-2341	-2340	-2561	-2491	-2255	-2544	-2451	-2408	-2497	-2362	-2440
    2716	2708	2560	2872	2659	2779	2808	2688	2703	2809	2827	2929	2658	2638	2655	2695	2803	3012	2571	2661	2481	2765	2808	2533	2594	2737	2599	2642	2822	2808	2702	2826
    2151	2205	2125	2156	1999	2193	2245	2071	2019	2059	1998	2128	2096	2043	2103	2226	2237	2223	2058	2182	2102	2076	2077	2293	2291	2056	2313	2198	2198	2293	2233	2265
    -2953	-2982	-2806	-3110	-2956	-3025	-3068	-2923	-2961	-3086	-3108	-3200	-2923	-2885	-2896	-2888	-2998	-3198	-2884	-2888	-2800	-3029	-3074	-2802	-2795	-2933	-2833	-2890	-3034	-3006	-2834	-3000
    -2387	-2481	-2372	-2400	-2295	-2441	-2506	-2304	-2275	-2337	-2275	-2404	-2357	-2291	-2347	-2416	-2431	-2411	-2371	-2413	-2422	-2337	-2340	-2565	-2492	-2256	-2546	-2449	-2407	-2491	-2366	-2440
    2718	2710	2561	2870	2663	2779	2808	2692	2703	2810	2828	2924	2659	2640	2651	2695	2806	3013	2571	2661	2478	2771	2808	2535	2593	2737	2602	2638	2821	2808	2705	2830
    2151	2206	2126	2161	2002	2193	2247	2068	2020	2059	1994	2130	2097	2044	2107	2221	2237	2223	2061	2184	2101	2073	2074	2296	2290	2058	2316	2197	2196	2290	2235	2263
    -2956	-2985	-2811	-3107	-2961	-3022	-3070	-2929	-2961	-3087	-3106	-3195	-2923	-2886	-2894	-2883	-3003	-3205	-2885	-2892	-2799	-3038	-3074	-2809	-2795	-2938	-2839	-2891	-3031	-3012	-2840	-3008
    -2385	-2483	-2371	-2401	-2297	-2443	-2508	-2302	-2276	-2340	-2271	-2407	-2360	-2293	-2349	-2415	-2433	-2410	-2375	-2415	-2422	-2336	-2342	-2567	-2494	-2259	-2549	-2450	-2406	-2490	-2368	-2438
    2721	2714	2568	2868	2668	2777	2813	2699	2707	2813	2827	2921	2660	2644	2651	2692	2812	3018	2575	2665	2480	2777	2808	2540	2593	2738	2608	2638	2822	2811	2712	2834
    2153	2208	2126	2161	2006	2199	2251	2068	2024	2063	1993	2133	2100	2047	2112	2226	2240	2222	2065	2184	2103	2069	2077	2296	2293	2058	2319	2198	2198	2289	2237	2261
    -2960	-2990	-2817	-3107	-2964	-3024	-3075	-2936	-2968	-3090	-3106	-3195	-2924	-2891	-2895	-2883	-3007	-3209	-2888	-2899	-2803	-3043	-3072	-2813	-2794	-2939	-2841	-2892	-3031	-3013	-2844	-3008
    -2392	-2486	-2372	-2401	-2302	-2450	-2513	-2304	-2282	-2343	-2273	-2412	-2365	-2297	-2358	-2424	-2433	-2410	-2376	-2415	-2424	-2335	-2344	-2569	-2496	-2260	-2551	-2452	-2411	-2494	-2368	-2437
    2725	2718	2572	2867	2670	2778	2816	2702	2713	2815	2827	2921	2660	2645	2653	2692	2812	3025	2577	2669	2482	2780	2804	2543	2590	2737	2607	2640	2820	2812	2712	2830
    2159	2212	2126	2163	2011	2208	2255	2071	2029	2066	1998	2138	2107	2052	2120	2237	2243	2222	2067	2184	2107	2071	2082	2301	2299	2061	2323	2202	2206	2296	2239	2264
    -2961	-2992	-2818	-3105	-2965	-3025	-3077	-2936	-2974	-3091	-3106	-3195	-2921	-2890	-2897	-2883	-3005	-3212	-2889	-2897	-2802	-3042	-3070	-2811	-2791	-2933	-2838	-2890	-3032	-3013	-2843	-3002
    -2393	-2490	-2370	-2405	-2303	-2456	-2515	-2310	-2286	-2346	-2277	-2416	-2373	-2299	-2366	-2434	-2439	-2408	-2379	-2413	-2431	-2337	-2350	-2572	-2503	-2262	-2558	-2455	-2420	-2500	-2372	-2440
    2724	2717	2569	2865	2667	2777	2814	2700	2719	2813	2826	2919	2656	2642	2655	2692	2811	3024	2577	2664	2481	2775	2804	2540	2586	2731	2602	2635	2821	2810	2707	2827
    2159	2215	2128	2165	2012	2209	2258	2077	2029	2068	2002	2140	2115	2051	2127	2242	2248	2221	2066	2183	2111	2075	2087	2304	2303	2063	2330	2207	2213	2302	2241	2269
    -2956	-2991	-2810	-3103	-2957	-3024	-3071	-2933	-2974	-3092	-3103	-3192	-2917	-2886	-2897	-2883	-3004	-3209	-2886	-2891	-2800	-3034	-3067	-2807	-2785	-2927	-2828	-2885	-3031	-3011	-2834	-3001
    -2393	-2491	-2372	-2405	-2303	-2454	-2516	-2315	-2286	-2347	-2281	-2413	-2380	-2298	-2370	-2436	-2440	-2408	-2376	-2414	-2429	-2340	-2351	-2575	-2501	-2263	-2563	-2461	-2422	-2504	-2372	-2446
    2717	2712	2561	2861	2659	2774	2808	2695	2714	2812	2822	2912	2654	2635	2655	2689	2810	3019	2573	2656	2480	2765	2800	2532	2582	2723	2592	2631	2820	2806	2699	2824
    2158	2215	2127	2162	2008	2201	2255	2080	2027	2067	2002	2135	2116	2046	2128	2242	2248	2219	2064	2182	2108	2075	2086	2302	2297	2061	2334	2208	2211	2300	2241	2269
    -2947	-2984	-2803	-3099	-2947	-3018	-3066	-2925	-2967	-3091	-3100	-3184	-2915	-2878	-2897	-2881	-3003	-3201	-2883	-2881	-2798	-3023	-3065	-2798	-2781	-2918	-2821	-2881	-3028	-3001	-2826	-2997
    -2389	-2489	-2368	-2398	-2298	-2443	-2510	-2316	-2280	-2342	-2277	-2405	-2375	-2290	-2364	-2432	-2439	-2405	-2374	-2412	-2424	-2338	-2349	-2572	-2494	-2261	-2565	-2460	-2418	-2499	-2370	-2443
    2712	2707	2555	2857	2649	2769	2804	2688	2708	2814	2821	2906	2651	2627	2655	2688	2809	3016	2570	2653	2476	2759	2798	2529	2577	2721	2590	2631	2815	2800	2691	2823
    2154	2208	2124	2153	2004	2191	2250	2077	2022	2059	1996	2126	2109	2037	2120	2233	2242	2218	2060	2182	2098	2076	2082	2298	2287	2059	2331	2205	2206	2294	2236	2265
    -2947	-2982	-2800	-3095	-2940	-3015	-3065	-2926	-2960	-3092	-3100	-3182	-2914	-2874	-2897	-2882	-3003	-3202	-2883	-2884	-2799	-3022	-3064	-2800	-2781	-2925	-2826	-2885	-3026	-3004	-2823	-2999
    -2386	-2480	-2364	-2393	-2295	-2438	-2508	-2311	-2277	-2335	-2269	-2401	-2368	-2284	-2356	-2423	-2430	-2406	-2372	-2411	-2417	-2339	-2345	-2567	-2485	-2257	-2561	-2454	-2414	-2493	-2365	-2437
    2713	2706	2555	2857	2648	2769	2808	2694	2701	2814	2822	2909	2652	2628	2656	2691	2812	3013	2573	2655	2482	2761	2798	2532	2581	2730	2598	2634	2814	2805	2691	2825
    2152	2201	2118	2151	2000	2190	2248	2073	2022	2055	1990	2124	2105	2033	2112	2225	2235	2217	2061	2179	2094	2075	2079	2291	2282	2055	2323	2198	2201	2289	2233	2258
    -2952	-2982	-2802	-3098	-2943	-3017	-3072	-2932	-2958	-3095	-3101	-3187	-2917	-2879	-2899	-2885	-3004	-3207	-2887	-2889	-2806	-3029	-3066	-2806	-2785	-2935	-2833	-2892	-3025	-3011	-2824	-3002
    -2386	-2476	-2363	-2394	-2292	-2440	-2507	-2306	-2278	-2334	-2266	-2401	-2365	-2282	-2351	-2417	-2425	-2408	-2372	-2410	-2410	-2338	-2341	-2559	-2480	-2255	-2550	-2451	-2409	-2493	-2363	-2434
    2720	2708	2558	2862	2650	2773	2815	2700	2703	2815	2824	2915	2656	2635	2657	2692	2811	3020	2577	2661	2488	2768	2802	2539	2583	2740	2602	2643	2814	2813	2693	2830
    2152	2200	2117	2156	1998	2194	2250	2069	2021	2057	1989	2129	2104	2035	2108	2220	2232	2221	2061	2179	2092	2076	2077	2286	2279	2054	2317	2199	2201	2292	2233	2259
    -2956	-2986	-2804	-3104	-2945	-3024	-3078	-2935	-2960	-3093	-3102	-3196	-2919	-2884	-2898	-2887	-3004	-3209	-2892	-2889	-2811	-3033	-3069	-2810	-2787	-2941	-2837	-2896	-3026	-3021	-2827	-3005
    -2386	-2477	-2359	-2399	-2289	-2444	-2510	-2304	-2275	-2338	-2266	-2407	-2363	-2285	-2350	-2415	-2425	-2409	-2374	-2410	-2413	-2341	-2342	-2555	-2481	-2252	-2547	-2450	-2412	-2491	-2367	-2435
    2723	2711	2560	2868	2652	2780	2820	2699	2706	2814	2826	2923	2659	2640	2656	2694	2810	3026	2581	2662	2492	2772	2806	2541	2587	2743	2606	2648	2817	2824	2696	2831
    2154	2203	2117	2158	1998	2196	2252	2070	2019	2063	1993	2133	2102	2039	2111	2221	2231	2222	2060	2180	2095	2079	2076	2285	2282	2051	2314	2197	2205	2293	2237	2262
    -2957	-2988	-2806	-3110	-2946	-3030	-3080	-2933	-2964	-3092	-3107	-3203	-2923	-2890	-2899	-2889	-3000	-3214	-2891	-2890	-2812	-3037	-3072	-2811	-2790	-2942	-2835	-2902	-3028	-3027	-2829	-3006
    -2387	-2481	-2362	-2400	-2290	-2446	-2514	-2307	-2273	-2343	-2273	-2410	-2366	-2289	-2352	-2416	-2423	-2410	-2371	-2410	-2417	-2343	-2340	-2556	-2486	-2253	-2545	-2450	-2416	-2493	-2369	-2437
    2723	2714	2562	2871	2654	2785	2818	2701	2710	2813	2831	2930	2661	2646	2658	2698	2806	3028	2579	2659	2494	2774	2808	2541	2591	2739	2603	2648	2821	2826	2700	2828
    2152	2206	2121	2157	1997	2198	2258	2074	2017	2068	1995	2134	2102	2041	2113	2226	2233	2221	2060	2178	2100	2079	2076	2285	2288	2052	2314	2196	2206	2292	2239	2262
    -2958	-2991	-2810	-3113	-2949	-3034	-3077	-2938	-2968	-3093	-3112	-3208	-2925	-2894	-2903	-2895	-2998	-3214	-2891	-2888	-2813	-3036	-3074	-2810	-2794	-2938	-2834	-2900	-3032	-3024	-2832	-3001
    -2389	-2483	-2366	-2398	-2292	-2447	-2518	-2311	-2273	-2348	-2274	-2410	-2362	-2289	-2353	-2419	-2428	-2408	-2371	-2412	-2421	-2343	-2343	-2560	-2492	-2257	-2549	-2451	-2417	-2496	-2372	-2438
    2722	2715	2564	2873	2658	2788	2815	2706	2711	2815	2836	2932	2663	2645	2664	2703	2802	3028	2577	2659	2491	2774	2807	2539	2592	2740	2602	2649	2821	2824	2700	2828
    2156	2209	2125	2155	2002	2200	2263	2076	2021	2068	1999	2134	2102	2041	2113	2226	2240	2220	2061	2184	2104	2079	2081	2292	2293	2060	2319	2202	2208	2298	2239	2265
    -2959	-2991	-2811	-3111	-2951	-3035	-3073	-2943	-2968	-3094	-3113	-3206	-2924	-2891	-2906	-2899	-2997	-3215	-2887	-2890	-2811	-3035	-3073	-2810	-2796	-2940	-2835	-2901	-3034	-3023	-2833	-3003
    -2392	-2486	-2372	-2398	-2296	-2449	-2524	-2313	-2280	-2349	-2276	-2413	-2364	-2290	-2356	-2422	-2436	-2408	-2375	-2417	-2424	-2343	-2347	-2565	-2497	-2263	-2552	-2457	-2418	-2504	-2370	-2441
    2724	2714	2565	2870	2661	2786	2810	2708	2711	2814	2835	2928	2659	2640	2664	2705	2805	3025	2575	2657	2489	2769	2807	2537	2594	2738	2603	2646	2821	2818	2701	2827
    2161	2212	2130	2160	2007	2204	2265	2078	2030	2071	2002	2137	2105	2044	2115	2231	2249	2221	2066	2189	2106	2079	2083	2298	2299	2066	2322	2208	2208	2304	2240	2267
    -2958	-2987	-2809	-3107	-2953	-3030	-3068	-2941	-2967	-3091	-3113	-3201	-2918	-2882	-2902	-2894	-2997	-3212	-2884	-2887	-2804	-3029	-3070	-2810	-2790	-2938	-2830	-2897	-3028	-3019	-2830	-3004
    -2395	-2490	-2376	-2402	-2302	-2453	-2524	-2316	-2288	-2351	-2281	-2415	-2370	-2293	-2359	-2426	-2439	-2411	-2376	-2421	-2423	-2346	-2348	-2571	-2499	-2267	-2550	-2461	-2417	-2505	-2369	-2444
    2721	2707	2561	2864	2660	2780	2805	2702	2711	2811	2832	2920	2653	2631	2657	2695	2803	3020	2572	2655	2480	2761	2803	2539	2585	2732	2595	2640	2815	2815	2696	2828
    2159	2213	2132	2161	2008	2204	2264	2079	2034	2072	2003	2138	2110	2046	2118	2233	2249	2223	2066	2190	2105	2083	2085	2299	2298	2066	2322	2207	2207	2301	2239	2268
    -2953	-2981	-2802	-3100	-2952	-3025	-3063	-2932	-2968	-3089	-3111	-3192	-2913	-2875	-2895	-2883	-2996	-3203	-2882	-2881	-2799	-3019	-3067	-2806	-2785	-2926	-2824	-2888	-3025	-3012	-2823	-3000
    -2391	-2488	-2374	-2401	-2298	-2450	-2519	-2315	-2286	-2351	-2279	-2416	-2371	-2295	-2359	-2429	-2441	-2410	-2375	-2417	-2426	-2346	-2348	-2568	-2494	-2263	-2553	-2457	-2414	-2498	-2369	-2440
    2716	2701	2556	2856	2655	2775	2801	2694	2712	2807	2830	2912	2648	2628	2651	2686	2802	3015	2569	2651	2476	2756	2800	2535	2581	2725	2590	2634	2812	2810	2688	2828
    2156	2209	2128	2159	2004	2198	2258	2076	2029	2068	1999	2139	2110	2045	2119	2235	2246	2220	2061	2185	2106	2082	2081	2293	2289	2059	2319	2201	2200	2290	2235	2261
    -2951	-2976	-2801	-3096	-2949	-3022	-3062	-2928	-2970	-3087	-3109	-3187	-2910	-2875	-2893	-2878	-2995	-3201	-2883	-2881	-2798	-3022	-3067	-2805	-2782	-2924	-2822	-2885	-3024	-3009	-2818	-3002
    -2388	-2484	-2370	-2399	-2295	-2442	-2512	-2312	-2281	-2344	-2274	-2416	-2371	-2292	-2359	-2429	-2435	-2404	-2369	-2411	-2425	-2342	-2345	-2562	-2485	-2254	-2551	-2451	-2410	-2486	-2363	-2432
    2717	2702	2557	2855	2657	2775	2805	2692	2714	2808	2829	2912	2648	2630	2655	2685	2802	3012	2573	2651	2481	2759	2802	2533	2581	2724	2593	2634	2813	2808	2686	2827
    2152	2206	2125	2157	2002	2191	2250	2076	2024	2062	1995	2138	2106	2041	2119	2233	2240	2213	2053	2175	2105	2075	2078	2288	2280	2049	2317	2196	2198	2280	2230	2251
    -2952	-2980	-2805	-3098	-2954	-3023	-3069	-2931	-2970	-3089	-3108	-3190	-2912	-2879	-2901	-2881	-2996	-3201	-2887	-2885	-2804	-3026	-3068	-2804	-2783	-2925	-2828	-2887	-3024	-3009	-2820	-3003
    -2384	-2483	-2371	-2397	-2293	-2436	-2504	-2312	-2276	-2338	-2271	-2414	-2365	-2288	-2357	-2426	-2431	-2399	-2362	-2404	-2422	-2339	-2343	-2560	-2479	-2249	-2546	-2449	-2406	-2482	-2361	-2428
    2720	2707	2562	2860	2663	2776	2811	2697	2714	2810	2829	2916	2652	2633	2662	2691	2798	3015	2575	2657	2485	2764	2802	2534	2582	2728	2599	2639	2813	2806	2689	2828
    2150	2206	2131	2155	2000	2186	2243	2077	2022	2056	1994	2138	2105	2038	2114	2230	2240	2213	2051	2175	2104	2074	2079	2289	2278	2049	2315	2197	2201	2283	2231	2254
    -2955	-2987	-2812	-3104	-2958	-3024	-3072	-2935	-2967	-3090	-3107	-3194	-2917	-2882	-2906	-2887	-2993	-3203	-2890	-2890	-2806	-3031	-3071	-2807	-2788	-2932	-2833	-2893	-3024	-3009	-2825	-3003
    -2385	-2483	-2379	-2396	-2293	-2434	-2500	-2313	-2277	-2335	-2271	-2416	-2367	-2285	-2353	-2424	-2435	-2400	-2363	-2406	-2424	-2334	-2344	-2561	-2484	-2252	-2548	-2449	-2413	-2486	-2364	-2432
    2720	2714	2572	2866	2668	2777	2814	2701	2713	2812	2830	2919	2656	2636	2666	2696	2800	3016	2579	2658	2485	2769	2807	2537	2588	2734	2602	2641	2815	2806	2695	2827
    2150	2206	2136	2157	2000	2188	2240	2078	2023	2056	1992	2141	2105	2037	2111	2231	2245	2214	2053	2178	2105	2070	2077	2292	2287	2054	2316	2198	2207	2289	2232	2262
    -2956	-2993	-2818	-3108	-2965	-3026	-3073	-2938	-2969	-3091	-3109	-3198	-2920	-2885	-2908	-2891	-2995	-3207	-2890	-2890	-2803	-3036	-3071	-2809	-2790	-2938	-2832	-2893	-3026	-3010	-2827	-3002
    -2385	-2483	-2381	-2399	-2295	-2438	-2498	-2313	-2277	-2337	-2271	-2417	-2367	-2284	-2352	-2427	-2438	-2405	-2365	-2410	-2424	-2336	-2341	-2562	-2489	-2258	-2548	-2450	-2417	-2494	-2363	-2440
    2721	2721	2574	2869	2671	2780	2814	2703	2715	2815	2831	2923	2659	2640	2665	2700	2804	3019	2579	2659	2482	2773	2806	2539	2592	2741	2602	2639	2818	2809	2698	2827
    2152	2208	2139	2160	2005	2191	2242	2077	2025	2060	1993	2141	2109	2036	2113	2236	2247	2218	2058	2181	2109	2072	2077	2291	2294	2062	2320	2201	2209	2295	2234	2269
    -2953	-2997	-2816	-3110	-2962	-3028	-3073	-2938	-2968	-3093	-3107	-3199	-2920	-2886	-2904	-2893	-3000	-3207	-2893	-2888	-2801	-3035	-3071	-2807	-2795	-2942	-2835	-2887	-3032	-3007	-2830	-2999
    -2388	-2483	-2383	-2401	-2300	-2442	-2503	-2315	-2281	-2341	-2273	-2418	-2373	-2284	-2356	-2432	-2442	-2411	-2372	-2413	-2430	-2337	-2342	-2561	-2496	-2265	-2552	-2456	-2418	-2499	-2367	-2447
    2719	2722	2570	2869	2670	2782	2815	2699	2715	2814	2829	2925	2658	2638	2662	2699	2809	3023	2580	2657	2481	2772	2805	2538	2594	2743	2603	2635	2823	2807	2698	2827
    2151	2206	2138	2161	2008	2197	2244	2080	2027	2065	1994	2141	2109	2039	2116	2239	2249	2224	2062	2185	2110	2075	2077	2291	2296	2067	2320	2206	2207	2299	2234	2273
    -2952	-2999	-2812	-3111	-2963	-3032	-3076	-2934	-2970	-3092	-3107	-3205	-2919	-2886	-2903	-2893	-3003	-3210	-2891	-2886	-2800	-3035	-3071	-2809	-2792	-2941	-2835	-2887	-3035	-3006	-2829	-3003
    -2388	-2481	-2382	-2402	-2304	-2443	-2505	-2316	-2283	-2345	-2275	-2416	-2372	-2288	-2357	-2432	-2443	-2413	-2377	-2415	-2430	-2338	-2343	-2560	-2496	-2268	-2552	-2459	-2418	-2501	-2367	-2449
    2716	2722	2563	2870	2668	2785	2815	2696	2712	2813	2829	2930	2654	2637	2660	2700	2813	3020	2579	2653	2480	2768	2805	2537	2590	2737	2604	2633	2826	2802	2697	2830
    2154	2202	2134	2160	2009	2195	2246	2081	2028	2067	1998	2136	2106	2038	2116	2237	2249	2223	2065	2183	2109	2071	2076	2287	2291	2066	2318	2205	2207	2299	2234	2272
    -2950	-2996	-2804	-3109	-2958	-3032	-3072	-2931	-2968	-3091	-3108	-3206	-2914	-2884	-2901	-2890	-3006	-3209	-2889	-2883	-2799	-3029	-3073	-2807	-2789	-2934	-2834	-2887	-3035	-3002	-2829	-3008
    -2390	-2478	-2377	-2400	-2300	-2441	-2504	-2317	-2281	-2347	-2277	-2410	-2365	-2286	-2355	-2428	-2438	-2411	-2375	-2415	-2426	-2337	-2339	-2559	-2488	-2267	-2546	-2457	-2415	-2502	-2363	-2445
    2716	2716	2554	2868	2662	2784	2813	2692	2712	2810	2832	2929	2649	2636	2660	2694	2813	3020	2577	2652	2478	2763	2806	2535	2584	2731	2600	2635	2824	2803	2697	2834
    2158	2202	2130	2159	2005	2194	2246	2080	2026	2067	1998	2131	2100	2037	2113	2232	2243	2220	2063	2183	2106	2073	2073	2287	2286	2064	2313	2202	2204	2298	2230	2268
    -2950	-2993	-2795	-3109	-2951	-3033	-3067	-2927	-2965	-3089	-3108	-3204	-2909	-2883	-2898	-2888	-3009	-3206	-2887	-2883	-2799	-3025	-3071	-2806	-2786	-2930	-2831	-2888	-3036	-3006	-2829	-3010
    -2394	-2479	-2375	-2399	-2298	-2442	-2506	-2314	-2278	-2346	-2272	-2403	-2360	-2283	-2353	-2422	-2433	-2404	-2373	-2413	-2424	-2336	-2337	-2555	-2485	-2261	-2544	-2453	-2413	-2498	-2359	-2439
    2718	2716	2552	2868	2658	2784	2810	2691	2713	2811	2829	2927	2649	2636	2659	2692	2816	3015	2575	2655	2481	2759	2806	2536	2585	2729	2597	2636	2825	2808	2699	2836
    2161	2204	2129	2159	2000	2197	2246	2079	2021	2066	1990	2126	2094	2035	2110	2226	2236	2214	2058	2180	2104	2075	2071	2285	2284	2058	2313	2200	2201	2296	2227	2262
    -2956	-2992	-2799	-3110	-2951	-3033	-3071	-2928	-2969	-3092	-3107	-3201	-2912	-2882	-2901	-2886	-3007	-3202	-2884	-2889	-2800	-3026	-3069	-2809	-2783	-2930	-2824	-2890	-3032	-3013	-2829	-3011
    -2396	-2481	-2374	-2400	-2295	-2445	-2508	-2313	-2275	-2343	-2267	-2402	-2357	-2283	-2350	-2419	-2427	-2402	-2368	-2408	-2422	-2338	-2337	-2555	-2484	-2257	-2543	-2452	-2409	-2496	-2356	-2437
    2726	2716	2556	2871	2660	2786	2813	2693	2715	2815	2824	2923	2651	2635	2662	2692	2816	3013	2573	2661	2486	2763	2808	2540	2584	2730	2594	2640	2823	2813	2700	2834
    2160	2207	2129	2160	2003	2198	2248	2076	2018	2063	1989	2128	2098	2036	2107	2227	2235	2213	2057	2174	2105	2076	2075	2284	2286	2055	2315	2198	2200	2291	2226	2262
    -2962	-2992	-2804	-3113	-2952	-3033	-3074	-2932	-2970	-3096	-3099	-3198	-2913	-2879	-2902	-2885	-3009	-3200	-2885	-2891	-2809	-3031	-3073	-2814	-2787	-2933	-2828	-2895	-3032	-3019	-2833	-3010
    -2394	-2483	-2374	-2402	-2298	-2447	-2508	-2310	-2275	-2339	-2269	-2405	-2365	-2284	-2349	-2421	-2429	-2404	-2369	-2405	-2424	-2342	-2343	-2556	-2490	-2254	-2549	-2452	-2410	-2495	-2361	-2441
    2730	2714	2563	2873	2663	2784	2819	2696	2718	2817	2821	2921	2653	2631	2661	2691	2815	3014	2572	2660	2491	2770	2807	2547	2586	2737	2596	2643	2820	2819	2702	2835
    2158	2209	2128	2164	2005	2201	2249	2073	2019	2061	1996	2135	2107	2037	2106	2231	2237	2219	2058	2174	2103	2079	2080	2288	2291	2052	2318	2201	2201	2294	2230	2271
    -2960	-2990	-2807	-3113	-2956	-3031	-3077	-2934	-2973	-3096	-3098	-3199	-2915	-2881	-2900	-2886	-3007	-3203	-2884	-2889	-2812	-3036	-3073	-2821	-2788	-2938	-2829	-2897	-3030	-3021	-2834	-3008
    -2394	-2485	-2373	-2404	-2299	-2449	-2508	-2309	-2278	-2340	-2279	-2414	-2374	-2285	-2350	-2427	-2433	-2407	-2369	-2405	-2423	-2344	-2349	-2561	-2499	-2251	-2551	-2456	-2414	-2497	-2364	-2447
    2724	2714	2564	2869	2665	2781	2819	2698	2719	2813	2823	2924	2654	2632	2659	2693	2813	3015	2571	2656	2492	2771	2808	2550	2587	2736	2597	2643	2817	2818	2702	2833
    2160	2208	2129	2167	2005	2203	2248	2075	2023	2061	2003	2140	2114	2038	2110	2235	2243	2221	2059	2176	2103	2080	2084	2292	2298	2052	2319	2206	2205	2296	2235	2275
    -2956	-2989	-2807	-3107	-2955	-3027	-3075	-2935	-2972	-3092	-3101	-3200	-2916	-2881	-2898	-2886	-3001	-3206	-2880	-2885	-2809	-3036	-3072	-2821	-2787	-2935	-2828	-2894	-3026	-3020	-2833	-3009
    -2399	-2485	-2377	-2410	-2297	-2452	-2506	-2310	-2281	-2340	-2284	-2418	-2378	-2287	-2354	-2427	-2435	-2411	-2370	-2409	-2423	-2345	-2349	-2566	-2500	-2255	-2550	-2461	-2414	-2499	-2366	-2448
    2723	2711	2560	2861	2660	2776	2815	2698	2718	2810	2826	2922	2657	2631	2656	2691	2808	3019	2567	2653	2489	2770	2805	2551	2584	2734	2597	2643	2816	2818	2702	2833
    2165	2209	2132	2169	2005	2204	2247	2076	2026	2062	2005	2143	2115	2040	2114	2234	2244	2225	2064	2181	2107	2082	2083	2295	2302	2059	2322	2212	2205	2296	2239	2271
    -2957	-2988	-2803	-3102	-2951	-3022	-3070	-2936	-2970	-3089	-3106	-3199	-2919	-2880	-2897	-2885	-2999	-3206	-2878	-2883	-2805	-3033	-3071	-2820	-2784	-2934	-2830	-2893	-3026	-3016	-2834	-3007
    -2402	-2485	-2381	-2410	-2300	-2451	-2507	-2311	-2284	-2341	-2282	-2418	-2376	-2289	-2357	-2427	-2437	-2412	-2377	-2411	-2426	-2345	-2347	-2564	-2499	-2260	-2554	-2462	-2417	-2496	-2371	-2442
    2724	2712	2559	2861	2656	2775	2807	2700	2715	2807	2831	2922	2657	2633	2657	2691	2805	3020	2566	2654	2485	2768	2803	2547	2581	2733	2601	2640	2816	2810	2702	2830
    2165	2207	2135	2167	2006	2203	2248	2076	2028	2060	2002	2141	2111	2044	2116	2234	2242	2227	2068	2183	2107	2083	2077	2293	2296	2063	2319	2212	2206	2297	2240	2265
    -2958	-2990	-2802	-3102	-2946	-3023	-3065	-2938	-2967	-3085	-3106	-3200	-2917	-2882	-2898	-2888	-2996	-3207	-2877	-2887	-2799	-3031	-3063	-2815	-2776	-2934	-2833	-2892	-3023	-3009	-2831	-3003
    -2400	-2481	-2380	-2403	-2301	-2448	-2510	-2307	-2284	-2338	-2279	-2415	-2371	-2291	-2356	-2428	-2434	-2414	-2380	-2411	-2429	-2348	-2339	-2562	-2496	-2262	-2551	-2463	-2416	-2499	-2374	-2438
    2723	2713	2557	2860	2655	2774	2805	2700	2711	2802	2829	2923	2655	2633	2658	2694	2806	3019	2571	2657	2484	2767	2798	2540	2576	2734	2606	2641	2816	2806	2701	2828
    2163	2205	2132	2160	2008	2199	2249	2071	2028	2058	2000	2139	2106	2043	2114	2233	2240	2225	2068	2177	2108	2082	2070	2287	2294	2060	2316	2210	2204	2296	2243	2261
    -2956	-2989	-2800	-3102	-2948	-3024	-3066	-2938	-2965	-3081	-3104	-3199	-2915	-2884	-2899	-2891	-2999	-3208	-2886	-2890	-2805	-3030	-3063	-2809	-2776	-2934	-2838	-2894	-3029	-3007	-2834	-3002
    -2395	-2478	-2377	-2398	-2300	-2445	-2510	-2303	-2282	-2336	-2276	-2413	-2367	-2289	-2356	-2425	-2431	-2413	-2378	-2406	-2425	-2345	-2334	-2556	-2495	-2258	-2549	-2461	-2415	-2497	-2374	-2435
    2722	2713	2555	2860	2657	2777	2810	2701	2710	2800	2827	2922	2653	2638	2658	2698	2806	3020	2575	2660	2487	2766	2795	2536	2576	2736	2605	2644	2817	2805	2700	2829
    2157	2201	2132	2158	2006	2197	2250	2068	2024	2057	1996	2137	2104	2041	2112	2234	2236	2227	2062	2175	2104	2078	2068	2285	2293	2057	2316	2206	2205	2292	2242	2259
    -2955	-2987	-2800	-3102	-2950	-3027	-3073	-2936	-2964	-3079	-3104	-3200	-2915	-2887	-2900	-2895	-3000	-3208	-2889	-2893	-2808	-3030	-3061	-2806	-2781	-2938	-2837	-2897	-3030	-3006	-2834	-3005
    -2390	-2477	-2377	-2398	-2300	-2444	-2509	-2303	-2280	-2337	-2274	-2414	-2367	-2286	-2354	-2427	-2429	-2414	-2371	-2402	-2422	-2339	-2334	-2554	-2493	-2254	-2550	-2456	-2416	-2490	-2374	-2433
    2721	2711	2558	2860	2659	2781	2816	2698	2709	2802	2826	2922	2653	2637	2660	2703	2805	3020	2578	2662	2487	2765	2797	2532	2581	2736	2604	2643	2820	2802	2699	2827
    2152	2200	2130	2157	2006	2194	2249	2068	2022	2059	1993	2139	2104	2037	2111	2234	2237	2226	2055	2173	2100	2074	2070	2286	2290	2054	2319	2203	2204	2289	2241	2261
    -2952	-2989	-2805	-3102	-2951	-3032	-3075	-2935	-2963	-3084	-3102	-3200	-2915	-2885	-2900	-2900	-2995	-3213	-2886	-2892	-2805	-3032	-3062	-2806	-2784	-2940	-2834	-2899	-3028	-3007	-2830	-3004
    -2387	-2476	-2374	-2399	-2300	-2438	-2505	-2306	-2277	-2337	-2270	-2414	-2368	-2281	-2354	-2424	-2430	-2412	-2362	-2403	-2419	-2337	-2336	-2558	-2488	-2253	-2550	-2453	-2415	-2489	-2373	-2438
    2718	2713	2565	2862	2661	2785	2817	2698	2709	2807	2827	2924	2655	2634	2661	2705	2802	3028	2575	2663	2486	2768	2801	2539	2587	2740	2603	2649	2820	2804	2701	2830
    2152	2201	2125	2161	2006	2190	2244	2074	2019	2058	1991	2138	2105	2033	2111	2229	2241	2223	2052	2175	2101	2073	2071	2289	2284	2053	2320	2199	2205	2289	2240	2267
    -2954	-2992	-2813	-3105	-2957	-3033	-3075	-2936	-2964	-3090	-3106	-3204	-2920	-2881	-2904	-2901	-2996	-3216	-2887	-2891	-2805	-3032	-3069	-2813	-2789	-2939	-2835	-2901	-3030	-3007	-2836	-3005
    -2389	-2478	-2368	-2403	-2301	-2434	-2504	-2312	-2276	-2337	-2269	-2414	-2369	-2280	-2354	-2419	-2437	-2408	-2362	-2406	-2424	-2335	-2338	-2559	-2484	-2253	-2552	-2450	-2416	-2491	-2371	-2444
    2719	2719	2569	2865	2666	2785	2813	2701	2709	2814	2831	2931	2657	2632	2663	2705	2803	3031	2574	2663	2486	2771	2805	2546	2586	2741	2602	2650	2820	2806	2705	2832
    2155	2203	2122	2165	2006	2187	2244	2082	2020	2058	1990	2136	2105	2034	2113	2227	2246	2221	2051	2179	2106	2072	2075	2290	2281	2056	2318	2198	2205	2291	2237	2274
    -2955	-2997	-2815	-3106	-2959	-3030	-3069	-2937	-2964	-3096	-3109	-3208	-2919	-2879	-2904	-2898	-2997	-3217	-2884	-2894	-2804	-3033	-3069	-2817	-2784	-2940	-2833	-2901	-3028	-3007	-2835	-3009
    -2391	-2480	-2367	-2405	-2299	-2436	-2507	-2317	-2278	-2336	-2267	-2409	-2369	-2283	-2354	-2421	-2443	-2409	-2363	-2411	-2429	-2334	-2343	-2559	-2485	-2257	-2550	-2451	-2414	-2495	-2370	-2449
    2723	2721	2571	2864	2667	2780	2807	2703	2711	2817	2833	2932	2654	2629	2663	2702	2806	3026	2574	2663	2488	2767	2807	2547	2584	2739	2603	2645	2819	2804	2706	2835
    2155	2206	2123	2165	2002	2194	2247	2082	2023	2058	1986	2132	2108	2038	2114	2229	2252	2223	2053	2182	2112	2070	2081	2292	2288	2056	2319	2201	2204	2296	2237	2274
    -2958	-2996	-2814	-3105	-2959	-3028	-3066	-2940	-2965	-3098	-3112	-3207	-2917	-2878	-2904	-2892	-3002	-3213	-2885	-2894	-2810	-3029	-3073	-2817	-2786	-2940	-2833	-2897	-3027	-3006	-2836	-3011
    -2390	-2480	-2371	-2401	-2295	-2441	-2511	-2315	-2281	-2335	-2265	-2404	-2374	-2285	-2357	-2422	-2445	-2413	-2365	-2412	-2433	-2335	-2347	-2563	-2489	-2257	-2549	-2456	-2413	-2499	-2368	-2448
    2724	2717	2565	2863	2662	2780	2805	2704	2709	2818	2830	2928	2653	2630	2662	2695	2809	3021	2572	2662	2490	2764	2806	2546	2586	2739	2599	2642	2816	2803	2703	2834
    2155	2207	2129	2161	1999	2199	2252	2080	2028	2058	1988	2130	2111	2040	2116	2234	2254	2227	2053	2181	2112	2073	2083	2295	2291	2056	2316	2204	2204	2298	2237	2274
    -2961	-2989	-2808	-3102	-2952	-3027	-3068	-2939	-2965	-3094	-3108	-3201	-2917	-2879	-2905	-2887	-3001	-3206	-2883	-2892	-2809	-3028	-3072	-2816	-2790	-2938	-2829	-2892	-3028	-3003	-2834	-3006
    -2392	-2482	-2379	-2399	-2292	-2447	-2515	-2313	-2286	-2336	-2268	-2406	-2375	-2286	-2359	-2429	-2445	-2413	-2366	-2410	-2431	-2336	-2347	-2564	-2492	-2252	-2549	-2455	-2412	-2497	-2369	-2448
    2726	2711	2560	2863	2654	2782	2809	2702	2707	2813	2828	2922	2652	2632	2663	2694	2805	3015	2572	2660	2488	2763	2806	2543	2590	2735	2596	2637	2817	2799	2702	2829
    2155	2210	2135	2157	1997	2203	2254	2078	2031	2059	1991	2132	2110	2038	2116	2239	2251	2227	2053	2181	2107	2074	2081	2296	2289	2051	2317	2205	2203	2295	2236	2274
    -2961	-2982	-2802	-3103	-2944	-3029	-3072	-2937	-2962	-3091	-3106	-3196	-2916	-2879	-2903	-2885	-2993	-3203	-2881	-2891	-2805	-3030	-3068	-2813	-2789	-2935	-2825	-2887	-3025	-2999	-2830	-3004
    -2389	-2483	-2381	-2393	-2289	-2445	-2514	-2308	-2286	-2333	-2271	-2406	-2373	-2283	-2357	-2431	-2442	-2415	-2363	-2408	-2424	-2337	-2345	-2567	-2490	-2249	-2551	-2458	-2412	-2496	-2368	-2447
    2724	2706	2556	2864	2648	2782	2814	2701	2705	2808	2827	2918	2653	2633	2661	2694	2799	3017	2572	2658	2486	2769	2804	2544	2591	2732	2597	2634	2817	2797	2701	2828
    2151	2211	2133	2154	1993	2198	2249	2075	2027	2057	1992	2133	2104	2037	2116	2238	2248	2223	2051	2176	2103	2070	2076	2294	2286	2048	2319	2206	2202	2292	2234	2271
    -2962	-2981	-2801	-3105	-2939	-3029	-3075	-2935	-2960	-3085	-3107	-3193	-2918	-2883	-2904	-2887	-2991	-3203	-2885	-2887	-2804	-3031	-3069	-2812	-2791	-2928	-2831	-2884	-3029	-2999	-2832	-2999
    -2386	-2485	-2378	-2392	-2287	-2441	-2508	-2306	-2282	-2333	-2270	-2409	-2367	-2283	-2357	-2431	-2440	-2408	-2362	-2404	-2422	-2334	-2342	-2561	-2487	-2247	-2550	-2459	-2414	-2492	-2364	-2444
    2726	2708	2555	2866	2647	2781	2816	2699	2706	2804	2829	2917	2658	2636	2663	2695	2797	3019	2575	2657	2485	2768	2800	2544	2589	2729	2601	2636	2820	2800	2699	2825
    2150	2211	2129	2152	1993	2193	2242	2072	2024	2055	1989	2136	2101	2036	2114	2236	2244	2218	2050	2173	2099	2070	2075	2289	2282	2047	2315	2207	2202	2290	2228	2268
    -2962	-2985	-2801	-3107	-2943	-3027	-3075	-2932	-2964	-3085	-3107	-3194	-2924	-2886	-2904	-2888	-2990	-3208	-2888	-2885	-2805	-3033	-3067	-2811	-2788	-2928	-2834	-2891	-3033	-3003	-2828	-2999
    -2383	-2486	-2373	-2391	-2286	-2441	-2500	-2306	-2279	-2334	-2268	-2412	-2363	-2284	-2356	-2427	-2437	-2403	-2362	-2404	-2420	-2332	-2343	-2557	-2484	-2246	-2549	-2460	-2414	-2490	-2362	-2440
    2729	2710	2555	2867	2654	2779	2813	2695	2709	2805	2829	2920	2663	2639	2663	2696	2799	3018	2579	2654	2486	2769	2803	2537	2587	2727	2604	2639	2826	2804	2696	2824
    2145	2211	2122	2153	1993	2195	2236	2075	2020	2058	1988	2136	2099	2036	2109	2234	2245	2214	2050	2177	2099	2069	2078	2288	2283	2048	2317	2209	2205	2290	2230	2267
    -2963	-2987	-2800	-3106	-2948	-3025	-3072	-2929	-2966	-3083	-3106	-3198	-2926	-2888	-2904	-2887	-2991	-3209	-2890	-2886	-2808	-3032	-3069	-2806	-2788	-2929	-2838	-2895	-3035	-3011	-2828	-2999
    -2380	-2484	-2366	-2392	-2287	-2443	-2498	-2310	-2278	-2338	-2269	-2410	-2364	-2283	-2354	-2422	-2438	-2402	-2363	-2408	-2420	-2334	-2343	-2560	-2485	-2250	-2549	-2461	-2415	-2491	-2363	-2441
    2727	2712	2553	2867	2657	2776	2810	2693	2712	2807	2828	2924	2663	2640	2660	2692	2800	3021	2579	2655	2490	2769	2807	2533	2587	2730	2609	2644	2824	2812	2698	2825
    2143	2211	2119	2156	1993	2199	2239	2081	2024	2065	1992	2135	2101	2038	2111	2230	2247	2217	2052	2179	2100	2073	2078	2291	2286	2051	2318	2207	2208	2290	2234	2266
    -2961	-2987	-2799	-3106	-2954	-3023	-3069	-2928	-2969	-3088	-3107	-3200	-2927	-2886	-2902	-2884	-2994	-3209	-2890	-2885	-2811	-3031	-3072	-2804	-2790	-2932	-2842	-2895	-3032	-3016	-2832	-3001
    -2379	-2484	-2364	-2397	-2289	-2447	-2503	-2316	-2282	-2345	-2277	-2408	-2365	-2286	-2353	-2421	-2442	-2406	-2366	-2406	-2422	-2338	-2345	-2562	-2489	-2252	-2548	-2458	-2420	-2489	-2366	-2440
    2723	2713	2556	2867	2661	2777	2809	2693	2713	2814	2829	2927	2661	2639	2659	2690	2805	3023	2577	2656	2491	2769	2808	2534	2591	2733	2611	2641	2822	2817	2701	2827
    2145	2209	2119	2160	1993	2201	2245	2083	2026	2069	2002	2132	2100	2041	2111	2231	2249	2223	2055	2178	2100	2079	2079	2293	2288	2056	2313	2207	2210	2291	2234	2266
    2145	2209	2119	2160	1993	2201	2245	2083	2026	2069	2002	2132	2100	2041	2111	2231	2249	2223	2055	2178	2100	2079	2079	2293	2288	2056	2313	2207	2210	2291	2234	2266

  • Hi  ,

    CONVST Freq: 108KHz
    Input Frequency: 27KHz

    this looks familiar... Is this still the problem you had back in december?

    I guess you still don't hit the extrema of your sine wave, but looking at your data dump your sampling frequency now seem to be synchronized with your input frequency, and you are constantly hitting the same points of your input sine wave, like in the second picture in the other thread.

    So, what can you do? You can either rise your sampling frequency or lower your input frequency, so you get more samples per period. Remember, the AD7606C can do up to 1 Msps, so you have a lot of room left. If both frequencies are fixed and you have to get the peak voltages, then you can play around with the System Phase Calibration of the AD7606C, to shift around the sampling point, until you hit the maximum. Or you do the math, and reconstruct your sine wave from your samples.

    Regards,

    rehfi

  • Hi Rehfi,

    Thanks for your reply, actually I want to calculate the voltage from these samples. Could you suggest to me on this?
     
    " I am doubting what should I consider the value of Full Scale Range in the calculation formula."


    Please Note: I haven't made any configuration changes for the ADC IC. "

    I attempted to perform calculations using a full scale of 40V (for diff.) for the default configuration RANGE_CHx_CHx register (i.e., single-ended for +/-10V). However, I am observing a discrepancy of approximately 1.5V between the input I am giving to the ADC and the digital data output I am receiving from the ADC.

    At some points, the samples are hitting Min/Max. so for comparison, I am taking the min. & max. of these samples for a particular channel.

  • Hi  ,

    If you want to stick to the Min/Max method, you should get more samples per period, i.e. by raising you sampling frequency.

    If you want to do the math, FFT comes to mind, or something like this.

    When you are not sure how to correctly calculate voltages from your ADC readings, then remember: RANGE_CHx_CHx register default is 0x3, which is the ±10 V single-ended range. Look up the LSB value in Table 11, which is 305.2 µV for this range. With the first sample of your data dump we then get -2379 x 305.2 µV = -0,73 V. With the next value we get 2730 x 305.2 µV = 0,83 V. Together this would be 1,56 Vp-p, but remember that you most likely didn't hit the maximum.

    You should also consider to use a range more fitting to you signal, like the ±2.5 V range.

    Regards,

    rehfi

  • Hi Rehfi, 
    I have a doubt

    When measuring my ADC input at V1+ wrt GND I am observing ~1.4Vpp, similarly, at V1- wrt GND I am observing ~1.4Vpp. So, Input to ADC will be ~2.8Vpp.

    But, while capturing from ADC (Digital Data, as you said) ~1.56Vpp is calculated.

    I used the same formula of multiplying the digital data with 305.2 µV & took the min/max (assumed not hitting the max), I m observing ~1.74Vpp (less than 2.8Vpp)

    Why is this variation we are observing? How is the data captured inside ADC? Isn't ADC measuring inputs as (V1+) - (V1-)?
    Are we missing any configuration needs to be done?




     

Reply
  • Hi Rehfi, 
    I have a doubt

    When measuring my ADC input at V1+ wrt GND I am observing ~1.4Vpp, similarly, at V1- wrt GND I am observing ~1.4Vpp. So, Input to ADC will be ~2.8Vpp.

    But, while capturing from ADC (Digital Data, as you said) ~1.56Vpp is calculated.

    I used the same formula of multiplying the digital data with 305.2 µV & took the min/max (assumed not hitting the max), I m observing ~1.74Vpp (less than 2.8Vpp)

    Why is this variation we are observing? How is the data captured inside ADC? Isn't ADC measuring inputs as (V1+) - (V1-)?
    Are we missing any configuration needs to be done?




     

Children
  • Hi  ,

    I'm not sure how you think the ADC works. It takes discrete samples out of your input signal, it doesn't continuously scan the inputs (or even scans for the minimum and maximum inputs). Is' not like a mutlimeter that gives you a RMS value for an AC-voltage, or an oscilloscope (which, on the other hand, does exactly the same as the ADC, but way more faster. A really lot faster).

    I took some samples out of your dump, threw them into excel, and tried to fit a sine wave over it:

    The blue line are your samples, if the line is zero, no sample is taken. The orange line is my guess what you input signal is. The pattern repeats over the whole dump. You can clearly see that when the input sine wave has its maximum, you don't take a sample. You take your samples "at the wrong time".

    Above I already gave some advises how to tackle this problem. The easiest one is the lower the frequency of your input signal. Try it with 1 kHz and take a look at your samples, just to get a feeling how it works.

    Regards,

    rehfi

  • Hi Rehfi,

    We are using FFT now for calculating the ADC Output Vpp.

    Below is the observation

    1. Input Amp. 1Vpp @ 270Hz.
    Output Amp. of ADC plotted in GUI 1.757Vpp
    Expected O/P : 2Vpp

    The observed data amplitude is nearly matching.



    2. Input Amp. 2Vpp @ 27KHz.
    Output Amp. of ADC plotted in GUI 2.37Vpp
    Expected O/P : 4Vpp

    The observed data amplitude is nearly half.



    HSDC FFT Plot


    Can you comment on this why is this variation we are observing at higher freq.? 

    Note: Full scale as 20Vpp here.

  • When you take the minimum and maximum from a set of samples and use that to calculate the amplitude of your input signal, then you have to oversample a lot, or it will not reliably work. You see that in 1), you oversample a lot, and you get better results.

    You have to be aware that this method is also highly susceptible to noise. One noisy sample can ruin your whole measurement when its the maximum value.

    When you want to get an amplitude from just a couple of samples, you have to put in more effort, and do some math, or you will run into the same problem over and over again. The FFT was just an idea, not a solution. I can't help you with that, maybe somebody else chimes in.

    Good luck!

    rehfi