LTC2485
Production
The LTC2485 combines a 24-bit plus sign No Latency ΔΣ™ analog-to-digital converter with patented Easy Drive technology and I2C digital interface. The...
Datasheet
LTC2485 on Analog.com
Page 10 indicates that the Vcc should be bypassed with a 0.1uF and 1 uF caps. It says that the 1 uF should be Tantalum. Why is this?
Hello adamvs ,
Tantalums are preferred because the internal LDO needs to have a high-ESR capacitor to ensure stability across operating conditions. Well, this is not strictly tantalum, you can add in place a ceramic capacitor with a series resistor of maybe 5-10 ohms. But then, that would be an extra component added to the BOM.
Regards,
Yugel
Hi, On evaluation board you have ceramic 1u F capacitor. Can you check again if tantal is really mandatory?
Hi Aless ,
You may use the evaluation board schematic and BOM as a guide in designing your own board. While the tantalum capacitor is preferred for the reason Yugel mentioned, it is not mandatory.
Hope this helps.
Regards,
JC