Hello there,
I'm using a custom software for a AD5941 project, and I am a little confused on how to use the command FIFO (sequencer) as a true command FIFO, I have the following questions:
1. Can I use the command FIFO as a true FIFO, where I could write a command using only one register, in this case using the CMDFIFOWRITE register, writing more commands as needed?
2. If question 1 is yes, how can I configure this behavior? Because there is no option for command FIFO in the CMDDATACON register:

As of now the only way I to use the sequencer is to write each command manually into a specific SRAM memory address, like this:
CMDFIFOWADDR<= command_address
CMDFIFOWRITE <= command
then for the next command:
CMDFIFOWADDR<= incremented_command_address
CMDFIFOWRITE <= another_command