Post Go back to editing

Command FIFO

Thread Summary

The user asked if the AD5941 command FIFO can be used as a true FIFO by writing commands to a single register. The final answer clarifies that the command FIFO operates only in memory mode, requiring commands to be written to specific SRAM addresses. The Data FIFO, however, functions as a true FIFO. No configuration options for a true command FIFO are available in the CMDDATACON register.
AI Generated Content
Category: Datasheet/Specs
Product Number: ad594x

Hello there,

I'm using a custom software for a AD5941 project, and I am a little confused on how to use the command FIFO (sequencer) as a true command FIFO, I have the following questions:

1. Can I use the command FIFO as a true FIFO, where I could write a command using only one register, in this case using the CMDFIFOWRITE register, writing more commands as needed?

2. If question 1 is yes, how can I configure this behavior? Because there is no option for command FIFO in the CMDDATACON register:

As of now the only way I to use the sequencer is to write each command manually into a specific SRAM memory address, like this:

CMDFIFOWADDR<= command_address

CMDFIFOWRITE <= command

then for the next command:

CMDFIFOWADDR<= incremented_command_address

CMDFIFOWRITE <= another_command