LTC2387-18
Production
The LTC2387-18 is a low noise, high speed, 18-bit 15Msps successive approximation register (SAR) ADC ideally suited for a wide range of applications. The...
Datasheet
LTC2387-18 on Analog.com
I'm using the DC718C data collection board together with P-scope to save ADC samples and load it into MATLAB. I encountered a problem, and this can be solved by collecting more data, maybe 10x more than the maximum size (131,072 samples).
Is there any way I can collect more than 131,072 samples with P-scope, or maybe another alternative?
Hi,
I will contact the product owner and get back to you.
Thanks,
Janine
Hello Abdelhakim ,
Can you send us a snapshot of your configuration in P-Scope? Also, may we know your specific application for this query? And if there are other things, we need to take note of?
Thanks and regards,
Jo
Hello NathanT ,
For now, I want to be able to calculate SINAD for an analog AM signal. The problem arises when the message signal strength is high; the SINAD varies by around 3dB from file to file. This is why I need more samples. Later im gonna do some test with a tetra signal.

Hello, Abdelhakim .
Here are some of my insights:
1) May we get another snapshot from the Pscope? Can you click the drop down in the size section?
2) Also, just wondering, have you made any modifications in the DC718C? Or are you using any other boards aside from our boards? Can we also get a photo of your setup? (e.g connections, power supply, etc.) This is to further asses the snapshot given.
3) We also noticed from your scope shot that you have a spurious signal at around 3.7 MHz. What are your thoughts on this? Is this unwanted? Or have you checked what caused this? If yes, can you tell us the specific reason on what caused this spurious signal?
As you can see from the figure from its datasheet, Fin used was 1MHz and samples used were only 32k. Then we should at least get a SINAD of around 94.6 dB based on these configurations.
But because of the spurious signal, it led to the degradation of the signal, resulting to a SINAD of around 24 dB. Removing the spurious signal should improve the SINAD by at least 50 dB. 
Thank you for your patience.
Warm regards,
Jo
Hey again,
Getting a SINAD of 94.6 is a bit tricky and depends on the testing gear. I'm using the LTC-2387-18 ADC with the DC718C and a DC2622A single-ended to differential converter, but this setup introduces some extra noise.
The spurious signal is just for testing. I want to see how well the ADC performs when there are blockers in the same frequency band I'm interested in. Planning to create a bit error rate curve to measure the performance drop caused by these blockers.
The signal I'm using to generate the BER curve is a tetra signal with a 36k bit rate. Given that I only have 131072 samples at a sampling rate of 15MHz, I end up with a duration of 8.7 milliseconds. This translates to 0.0087 seconds * 36,000 bits per second, resulting in 313 bits for my analysis.
which is too few bits to obtain a smooth and reliable BER curve.