Post Go back to editing

Is there a way to test EVAL-AD4134 in Minimum I/O mode using SDP-H1 board?

Category: Software
Product Number: AD4134

Hello,

We purchased EVAL-AD4134 and SDP-H1 boards and have managed to test them using the ACE software. Apart from a few weird things (e.g. data is slightly corrupted in slave mode at the start of the capture, when the sampling rate is 1 or 10 kHz), we managed to measure meaningful data. Our application requests using a Minimum I/O mode and thus we wanted to setup the EVAL-AD4134 to work in this specific mode, which would then also allow to test our design as well. Going through the EVAL-AD4134 setup guide I noticed that there are steps to do so, however in the same document under Limitations section it is saying that ACE software does not support Minimum I/O mode:

Given this, what is the best course of action for us to test the EVAL-AD4134 together with SDP-H1 in Minimum I/O mode?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.