Post Go back to editing

AD4130- 8 power down mode

Thread Summary

The user is experiencing issues with the AD4130 in WLCSP package, specifically with waking up the device from power-down mode and reading corrupted data from the DATA register. The final answer indicates that the device must be reset to exit power-down mode, as detailed in the AD4130-8 datasheet. The user's workaround of omitting the last write to the CTRL register (POWER_DOWN mode) helps but is not ideal.
AI Generated Content
Category: Hardware
Product Number: AD4130- 8
Hi, I am using the AD4130 in the WLCSP package on my custom board. The standard way of operating is as follows:
  1.  Power on the device.
  2. Wait 2048us for the reset to perform.
  3. Soft reset the device (by writing 64 consecutive 1s to the device).
  4. Wait 2048us.
  5. Read the ID register content.
  6. SETUP registers:
    • CONTROL (SPI 4-wire, int_ref_en, data_status).
    • MISC (stby_refhole_en, stby_diagnostics_en).
    • ERR_EN(spi_write_err_en, spi_read_err_en, spi_ignore_err_en)
    • CONFIG (pga_gain).
    • FILTER (filter_mode_n = 2, fs = 2047).
    • CHANNEL (ainp, ainm, enable_m).
    • CONTROL (set single_con).
  7.  After the data_ready signal on the INT pin - I read data and status from the DATA register. If there is a master_err flag, I also read the ERRORS register and then write 0 to it to clear its content.
  8. SETUP registers:
    • CTRL (mode = STANDBY)
    • Wait 1ms
    • CTRL (mode = POWER_DOWN)
  9. Wait for some time (20sec) and then perform steps 1-8 again.
The first problem I've encountered is the fact that I can't wake up the device. The content of the ID reg is always corrupted. To fix this, I omit the last writing to the CTRL register (choosing POWER_DOWN mode). It helps, but it is not a solution that satisfies me.
Another problem is the content of the DATA register, which sometimes is not correct. 
Perhaps somebody can point out what I am doing wrong? Or does anyone have a similar problem with this ADC? Thank you in advance.