Post Go back to editing

AD7380 data and clock interface circuit config question

Thread Summary

The user inquires about the configuration of the AD7380 for 2-channel simultaneous sampling, noting the presence of 100-ohm resistors in series with SDOA and SDOB but not with SCLK. The final answer confirms that SCLK should be directly connected to the controller without a resistor to ensure fast SPI communication. An accompanying answer explains that the 100-ohm resistors on SDOA and SDOB help mitigate trace impedance issues for longer board designs, which is crucial for maintaining performance at the 4MSPS throughput rate.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD7380

I want to use AD7380 for 2 CH Simultaneous Sampling, per studied the spec, I found that in Spec Page 17, figure31, SDOA and SDOB had 100 Ohm Resister with series, but in SCLK, had no any R.

My question is that, if this config has some reasons behind? the data latency or CLK latency mismatch will be caused by this 100 ohm R there? I guess that the Data or CLK I/O designed with same circuit block, why the terminal is used with different ways?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.