Post Go back to editing

Using AD5941 to design a battery impedance measurement for 8V to 100V battery

Thread Summary

The user is modifying the CN0510 battery impedance measurement circuit to support 8V to 100V battery voltages. The final answer suggests changing the TIP31BG transistor to a higher voltage-rated one and confirms that a high-voltage, low-current SMT transistor can be used. The user encountered negative real impedance values when testing a 15V battery, which may be due to the reactive components at certain frequencies. The solution involves ensuring the correct high-voltage components are used and verifying the impedance calculation method.
AI Generated Content

Hi,

I am using AD5941 to design a battery impedance measurement circuit. I follow the reference design CN0510. But my target battery voltage will be 8V to 100V. May I know what modification need to achieve my task? Thank you.

Sam