I'm observing fft peak power on ACE being different from when it gets exported & plotted. Follow graph is a 1kHz signal measurement using AD4630-24.
ACE measures fundamental power -0.491dBFS.
When exported in csv file, the FFT plot (done in matlab) show fundamental power is -4.81dBFS. Then I came back to ACE plot and noticed that dot on fundamental, lying somewhere around 0dB (full scale), whereas the tone below it has a peak at around -4dB, which aligns with MATLAB plot. Why the small gap and difference?