I designed my own PCB based on EVAL-AD76XXEDZ, but I found on this board, the SNR of the AD7634 at 670KHz is only 96dB. I think it might be a problem with the board design.What are the ways to improve the performance? This is PCB design.
AD7634
Production
The AD7634 is an 18-bit charge redistribution successive approximation register (SAR), architecture analog-to-digital converter (ADC) fabricated on Analog...
Datasheet
AD7634 on Analog.com
MAX8632
Production
The MAX8632 integrates a synchronous-buck PWM controller to generate VDDQ, a sourcing and sinking LDO linear regulator to generate VTT, and a 10mA reference...
Datasheet
MAX8632 on Analog.com
I designed my own PCB based on EVAL-AD76XXEDZ, but I found on this board, the SNR of the AD7634 at 670KHz is only 96dB. I think it might be a problem with the board design.What are the ways to improve the performance? This is PCB design.
Hi BeginnerInAnalog ,
Here are some of my insights to your concern:


Please let me know if ever these insights will help you so that I could further assist you.
Thanks and regards,
Jo
Hi BeginnerInAnalog ,
To get the full performance with a board connected to a computer is quite tricky and sometimes it does not depend only on the layout but also on the setup.
Normally the Vref should be as close as possible to the ADC, supplies for the ADC should be as clean as possible and the PSRR of the amplifiers should be high enough to avoid introducing noise into the measurements.
you should also try to avoid noisy signals crossing sensitive paths.
In terms of the set-up, if you are reading the data with a laptop, try to use the laptop floating in battery mode and try to avoid using usb to read the data.
In my experience, the instrument used to generate the signal also introduces some noise into the system if there are ground loops, so I normally connect the ground of the PCB to the chassis of the instrument or protective earth.
Regards
Joan
thank you for your reply
thank you for your reply
I saw some of the ADI's EVAL board also contain the DESIGN & INTEGRATION FILE,does these files contain some PCB examples?
Hi BeginnerInAnalog ,
Yes. Some device's PCB designs are also included in these design files. You could try looking at it and use it as your reference as this were already made for the device's optimal performance.
Warm regards,
Jo