Post Go back to editing

LTC2380-24 and LTC2368-24 Multidevice Synchronization?

Thread Summary

The user inquired about synchronizing the sampling clock in the LTC2380-24 and LTC2368-24 ADCs for a 3-channel phase comparison application. The final answer indicates that these ADCs have independent sampling clocks and conversion times, making simultaneous conversion unguaranteed. The engineer suggested considering other Analog Devices products like the AD7380-4, AD4630-24/AD4632-24, and AD4858, which support multiple channel, simultaneous sampling. The user later decided to use the LTC2500 due to its digital filters and decimation capabilities.
AI Generated Content
Category: Hardware
Product Number: LTC2380-24, LTC2368-24

Hello,

Is there a way to synchronize the sampling clock in either the LTC2380-24 or the LTC2368-24?  The application is dictates 3 ADCs be synchronized to the main sampling clock.

Thanks,
Mike

Parents Reply Children
  • Hi  

    May I know your application for the 3 synchronized ADCs?

    As of now, please read these pages from respective datasheets.

    For LTC2380-24, refer to pages 25-27, (Chain Mode, Multiple Devices)

    For LTC2368-24, refer to pages 24-26, (Chain Mode, Multiple Devices)

    For your additional reference, you may check this link: Introduction to SPI Interface | Analog Devices

    Thank you.

    Regards,

    Red

  • Hello,

    Application is taking 3 channels of ADC and comparing phase of the input signal.  We require the sampling clocks on the ADCs to be in SYNC down to the individual clock.  Does using the convert pin align the internal sampling clocks of individual ADCs?

    Thanks,
    Mike

  • Hi  

    Each device has independent sampling clock and conversion time, (tconv). The tconv will also vary for each device, since there is a range for minimum and maximum conversion time (Please check the datasheet). Hence, considering your application, we cannot guarantee that the 3 independent ADCs will convert simultaneously.

    Please refer to the Normal Mode, Multiple Devices: page 26 for LTC2380-24 and page 25 for LTC2368-24.

    Also take note of these:

    1. The conversion is controlled by CNV. A rising edge on CNV will start a conversion and power up the device. Once a conversion has been initiated, it cannot be restarted until the conversion is complete. 

    2. Since SDO is shared, the RDL/SDI input of each ADC must be used to allow only one LTC2380-24 or LTC2368-24 to drive SDO at a time to avoid bus conflicts.

    3. Both devices have an internal clock that is trimmed to achieve a maximum conversion time.

    May I know your other requirements for your project? I can recommend other Analog Devices, which I think more suitable for an application which requires a multiple channel.

    Please check these links: 

    1. AD7380-4 (Rev. 0) (analog.com): The AD7380-4 is a 16-bit compatible, quad, simultaneous sampling, high speed, successive approximation register (SAR), analog-to-digital converters (ADC) operating from a 3.3 V power supply with throughput rates up to 4 MSPS. The differential analog input accepts a wide common-mode input voltage and is sampled and converted on the falling edge of CS.

    2. AD4630-24/AD4632-24 (Rev. B) (analog.com): The AD4630-24/AD4632-24 are two-channel, simultaneous sampling, Easy DriveTm, 2 MSPS or 500 kSPS successive approximation register (SAR) analog-to-digital converters (ADCs).

    3.AD4858 (Rev. 0) (analog.com): The AD4858 is a fully buffered, 8-channel simultaneous sampling, 20-bit, 1 MSPS data acquisition system (DAS) with differential, wide common-mode range inputs.

    Thank you.

    Kind regards,

    Red

  • Hi Red,

    Thank you for the detailed response and suggestions.  I think we are leaning towards using the LTC2500 because of the digital filters and decimation.

    Thank you for your time.
    Mike

  • Hi  

    You are welcome. Good to know that you've already decided which device to be used.

    Thanks.

    regards,

    Red

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.