Hello, I'm trying to determine whether the AD7124-8 is correct for my application.
I am attempting to hook up 8 load cells, each with their own differential output such that I can make use of 8 differential channels on the ad7124-8. I want to sample each channel at 100 hz.
The load cells are roughly 1mV/V and the excitation will be 3.3V. So I'm planning on using a gain of 128 for each load cell.
Assuming no filtering, can I achieve a sampling rate of 100 samples per second for each of the 8 load cells using the ad7124-8?
What would be the maximum samples per second I could achieve assuming I am continuously measuring and cycling through 8 differential channels?
Perhaps I missed it, but in the data sheet I only see data for continuous converting on a single channel, I'm curious to know the expected sampling rate when cycling across multiple channels.