Post Go back to editing

DC2390A-A Applications

Category: Hardware

Hello,

I am currently working on DC2390A-A board along with a DE10 Standard FPGA.

There are two outputs of LTC2500, one is a 32-bit filtered output, and the other is a 32-bit no latency composite code output. I have a couple of questions regarding it.

1) Do I need to program the control word to use the 32-bit output as a "Conventional SAR Operation (N=1)" application provided in the LTC2500-32 datasheet? (Page 40) If yes, what to provide?

2) Do I need to program the control word to use the 32-bit no latency output data? (Page 45) If yes, what to provide?

I have attached the link to the datasheet to this message for your reference.

Link: LTC2500-32 - 32-Bit Oversampling ADC with Configurable Digital Filter (analog.com)

Thanks in advance for your time and consideration.

Regards