Post Go back to editing

I encountered issues while using the AD7634

Thread Summary

The user observed output discontinuity in the AD7634 ADC when operating at 670KSPS with a 120mV, 100Hz signal. The support engineer requested clarification on the data capture method, axis labels, and suggested checking the supply voltages, particularly the negative supply voltage, to ensure optimal performance. The engineer also inquired about the specific application to recommend better-suited products.
AI Generated Content
Category: Hardware
Product Number: AD7634

Translation: 

When the operating frequency of the AD7634 is 670KSPS, when a small signal of about 120mV (100Hz) is applied, there is a discontinuity in the output. why is this happening

当AD7634的工作频率为670KSPS时,施加约120mV(100Hz)的小信号时,输出中存在一段不连续性。为什么会这样?

Edit Notes

Translated
[edited by: GenevaCooper at 1:54 PM (GMT -5) on 15 Nov 2023]