Post Go back to editing

I encountered issues while using the AD7634

Thread Summary

The user observed output discontinuity in the AD7634 ADC when operating at 670KSPS with a 120mV, 100Hz signal. The support engineer requested clarification on the data capture method, axis labels, and suggested checking the supply voltages, particularly the negative supply voltage, to ensure optimal performance. The engineer also inquired about the specific application to recommend better-suited products.
AI Generated Content
Category: Hardware
Product Number: AD7634

Translation: 

When the operating frequency of the AD7634 is 670KSPS, when a small signal of about 120mV (100Hz) is applied, there is a discontinuity in the output. why is this happening

当AD7634的工作频率为670KSPS时,施加约120mV(100Hz)的小信号时,输出中存在一段不连续性。为什么会这样?

Edit Notes

Translated
[edited by: GenevaCooper at 1:54 PM (GMT -5) on 15 Nov 2023]
Parents
  • Hi  ,

    Based on your query, I have the following questions and concerns:


    1) Based on your snapshot, did you get it from the first data capture? Or from a continuous data capture?

    2) This is a continuation of my first concern, what are the labels of this each axis?

    3) You can refer to this section on its datasheet

    4) You can try checking its supply voltages, specifically its negative supply voltage. You can refer to the image below as your reference. These are from its datasheet and user guide. It is still best to follow what it's on these pages since these were tested to be on its optimal performance.


    Also, may we know what is your specific application? Since you are using a low throughput rate device. Maybe we could suggest better products suitable for your specific application.

    Regards,
    Jo

Reply
  • Hi  ,

    Based on your query, I have the following questions and concerns:


    1) Based on your snapshot, did you get it from the first data capture? Or from a continuous data capture?

    2) This is a continuation of my first concern, what are the labels of this each axis?

    3) You can refer to this section on its datasheet

    4) You can try checking its supply voltages, specifically its negative supply voltage. You can refer to the image below as your reference. These are from its datasheet and user guide. It is still best to follow what it's on these pages since these were tested to be on its optimal performance.


    Also, may we know what is your specific application? Since you are using a low throughput rate device. Maybe we could suggest better products suitable for your specific application.

    Regards,
    Jo

Children
No Data