KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD7766
Production
The AD7766/AD7766-1/AD7766-2 are high performance,
24-bit, oversampled SAR analog-to-digital converters (ADCs).
The AD7766/AD7766-1/AD7766-2 combine the...
Datasheet
AD7766 on Analog.com
I can't understand digital filters inside ADC....
Modulators (sigma-delta) works with higher frequencies than the output data rate, so I need low-pass filter before decimation. Ok, it's clear.
Let's say I have a vibration sensor, range DC to 4kHz, frequency response as 2th order low-pass filter with pole at (-3dB) 4kHz, so flat frequency response until cut-off frequency.
I need ODR at 1000SPS, 24 bit, so sigma-delta or SAR ADC, let's suppose 1000 SPS would be available from ADC as ODR decimation factor.
Taking a look to available ADCs I always see sinc as digital filter after modulator (except for LTC2500).... but sinc filter hasn't flat response (AN-0979, fig.1-2, LTC2500 datasheet, fig.27), so I will not expect flat frequency response from ADC at selected ODR.
AD7766 (AD7766 datasheet, fig. 32, 33, 34) shows flat response, so I suppose it would be overall frequency response including sinc, right?
I am confused about sinc after modulator and flat frequency response I can find on datasheets....
BTW:
LTC2500 sinc filter coefficients are correct? I can see only ones....