KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
AD7766
Production
The AD7766/AD7766-1/AD7766-2 are high performance,
24-bit, oversampled SAR analog-to-digital converters (ADCs).
The AD7766/AD7766-1/AD7766-2 combine the...
Datasheet
AD7766 on Analog.com
I can't understand digital filters inside ADC....
Modulators (sigma-delta) works with higher frequencies than the output data rate, so I need low-pass filter before decimation. Ok, it's clear.
Let's say I have a vibration sensor, range DC to 4kHz, frequency response as 2th order low-pass filter with pole at (-3dB) 4kHz, so flat frequency response until cut-off frequency.
I need ODR at 1000SPS, 24 bit, so sigma-delta or SAR ADC, let's suppose 1000 SPS would be available from ADC as ODR decimation factor.
Taking a look to available ADCs I always see sinc as digital filter after modulator (except for LTC2500).... but sinc filter hasn't flat response (AN-0979, fig.1-2, LTC2500 datasheet, fig.27), so I will not expect flat frequency response from ADC at selected ODR.
AD7766 (AD7766 datasheet, fig. 32, 33, 34) shows flat response, so I suppose it would be overall frequency response including sinc, right?
I am confused about sinc after modulator and flat frequency response I can find on datasheets....
BTW:
LTC2500 sinc filter coefficients are correct? I can see only ones....
Hi Killertechno ,
Please take note that if your input signal can reach up to 4kHz, the ODR must be twice or greater.
Regarding the frequency response of the filters, the figures 32, 33, and 34 are showing the overall frequency response up to the ODR.
The sinc filter response you are referring to showing notches are plotted in multiples of the ODR, e.g. ODR, 2ODR, 3ODR.
Hi NathanT ,
Please help advise on the LTC2500 sinc filter coefficients.
Thanks,
Janine
Hi Killertechno ,
You can refer to this, as sincN filter has the following equation:
![]()
Where N is the order of the sinc filter and DF is down sampling factor. If for example, we calculate the coefficients for sinc1 and DF=4 then we can yield the following equation:
![]()
So, yes. The coefficients for Sinc1 are all 1s.