Post Go back to editing

AD7928 Interfacing with Arduino

Category: Hardware
Product Number: AD7928
Software Version: Arduino - VS Code

Hello, I am trying to interface AD7928 with Teensy (Arduino Framewok) using the SPI Communication. My goal is to read 8 sensors with this ADC

  1. I set the SPI Mode to 2 for this communication as the Data clocks out on the DIN line at the falling SCLK cycles
  2. I wrote the Poweup mode function as shown in Figure 24 and Page 22 of the datasheet and towards the end I set the Control register to read channel 0 for the conversion.
  3. I do not intend to use the SEQ and Shadow at this point as they seemed to complicated for a beginner.
  4. I am following the Normal mode operation indicated in Fig 22 and the schematic in Figure 11.

I have the following function code to read all the sensors and update a global array that stores the analog value : ADCout[8] is the global array storing the the converted values.

The powerup mode already sets the channel address in the Control register to Vin0; hence at the end of the 7th iteration, the channel address is reset to Vin0;

void readAD7928All()
{ // By default read all 8 pins

 
  int digValue[8];

  u_int16_t ADC_Mask = 4095; // 0b0|AD2|AD1|AD0|0000 // Mask to isolate converted output

  // Step 1 : read channel 0 and move onto next until the end

  for (int itr = 0; itr < 8; itr++)
  {

    // Write Control Register for next and read the first channel

    byte Ctrlreg1_mask = 0b10000011;
    byte Ctrlreg1;
    byte channelBits;

    if (itr == 7)
    {
      channelBits = 0 << 2;                   // Channel Bit for next capture : reset channel bit to 0 for last channel
      Ctrlreg1 = Ctrlreg1_mask | channelBits; // Including ADD2-> ADD0
    }
    else
    {
      channelBits = (itr + 1) << 2;             // Channel Bit for next capture
      Ctrlreg1 = Ctrlreg1_mask | channelBits; // Including ADD2-> ADD0
    }

    // Byte 2: SHADOW | DON’TCARE | RANGE | CODING | - | - |- |-
    byte Ctrlreg2 = 0b00000011;

    u_int16_t CTRLReg = Ctrlreg1 << 4 | Ctrlreg2; // Control Register Stored as 16-bit

    // Transfer Begin
    SPI.beginTransaction(SPISettings(1000000, MSBFIRST, SPI_MODE2));

    // noInterrupts(); // disable interupts to prepare to send address data to the ADC.
    digitalWrite(ADCChipSel, LOW);
    delayMicroseconds(1);

    digValue[itr] = SPI.transfer16(CTRLReg<<4); // Transfer and capture the reading

    digitalWrite(ADCChipSel, HIGH);
    delayMicroseconds(1);

    // interrupts();
    SPI.endTransaction();

    // Transfer Complete
    digValue[itr] = digValue[itr] & ADC_Mask;
    ADCout[itr] = float(digValue[itr]) * 2.5 / 4096;
  }
 
}

The ADC output determined this way is very random. I even connected the 4 SPI channels to the Oscilloscope and I get random output from the ADC. I seek help here to improve my understanding and help me acquire the signals using this ADC

Thank you.

Yellow - CS; Turqoise - SCLK; Pink : DIN, Blue - Dout - I was trying to read channel 0

  • Hi  ,

    I'll contact the product owner and get back to you.

    Regards,
    Jo

  • Hello @Nathan T ,

    I partially have resolved the issue. Since I am interfacing with a microcontroller, according to page 20 and Figure 20 of the Datasheet, the VDrive has to be supplied with 3.3V and the ADD has to be supplied with 5V. I was mislead by the specification given in Page 7. Now I understand that VDrive sets the Logic High and Low when interacting with the microcontroller. The Digital high and low from Teensy are 3.3V and 0V. Hence, when I changed VDrive to 3.3V, I was able to record correct voltage values.

    Another query I have is VRefIn is mentioned to be strictly 2.5V. But the Absolute Maximum range for this value is ADD+0.3V. Could I still operate this with a 3.3V Reference or is it absolutely necessary to be held at 2.5V. Please let me know your thoughts on this issue.

    Regards,

    Sneha

  • Hi  ,

    Sorry for the late response. Regarding your query about VRefin, the device should have a 2.5 V voltage reference to have an optimal performance. Since the parameters shown in its specification table has a reference voltage of 2.5 V. You can also refer to its pin function description, on page 11.


    Let me know if you still have other concern so that I could further assist you.

    Regards,
    Jo

  • Hi ,

    I have a follow up question for the external ADC reference for this chip. Initially I was using the ADR4525 (this gives a PWM output) as the reference voltage for the AD7928 in hopes of getting a stable reading of the signal. However my signal read in was prettly noisy. I am curious about the kind of voltage reference (is it DC using an LDO or PWM) in chips that have an internal reference?

    Can I just use a DC 2.5V for this purpose and have a cleaner signal or do you have an other recommendations?

    Kind regards,

    Sneha

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.