AD4010
Recommended for New Designs
The AD4002/AD4006/AD4010 are high accuracy, high speed, low power, 18-bit, Easy Drive, precision successive approximation register (SAR) analog-to-digital...
Datasheet
AD4010 on Analog.com
Hey everyone,
I am struggling to setup the SPI interface and test the output for AD4010 ADC. The wiring in data sheet don't seem to be traditional SPI setups, I believe input for SCK and output for SDO are standard. For the CNV pin, how am i supposed to connect this? Do i tie it to the SCK pin? And the SDI pin im confused about how this is supposed to be wired, because traditionally this is NOT the CS pin. Even though the datasheet makes it seem like i have to connect CS from the host device to the ADC SDI. If someone can describe quite plainly exactly how to wire the 4 pins i would greatly appreciate it.
Thanks!
Matt
Hi Mgibson9 ,
Pardon for coming back late. I hope you are well. So, here are my insights to your concerns:
1) For CNV. You can refer to page 23 of its user guide. CNV is externally controlled; it acts as the chip select (CS) of the device.
2) Also, for its SDI, you can refer to its user guide as your reference.

Also, for a good reference, here is a link provided.
Introduction to SPI Interface | Analog Devices


Regards,
Jo