I'm contemplating using the LTC2358-16 in a system that is doing some high accuracy DC measurements coming from sensors. This converter seems like a really good choice.
I'm most concerned in relative accuracy of the channel measurements, i.e. the ratios of the values of different channels. So for example if input 1 is 1.5V and two is 3V, the accuracy of the ratio measurement (i.e. 0.5) is what I'm most interested in. The linearity and offset information will help me assess that, but I don't see any gain error info. I've seen specs in similar converters that give channel to channel gain matching numbers. This converter doesn't give a spec like that..
I see there's a full scale error listed as 0.1%. This seems similar to a TUE spec, but it seems pretty loose considering all the other accuracy specs are really tight (zero error is <700µ, INL < 1.5lsb etc..).
I also see there's a full scale error graph listed with a bunch of lines, which represent the channels. They don't seem to indicate which lines are which channels, or if this is just typical performance vs a max.
Is there any more information on these to help me assess the accuracy of the ratio measurement I'd be getting?
fixed typos
[edited by: PatrickAnalog at 3:17 PM (GMT -4) on 17 Oct 2023]