The FAQ doc for the AD4111/2/4/5 discusses the recommended values for the RC anti-alias filtering, but the fact that the resistors are in series with the internal burden resistor for current measurements means that 4-20 mA current loops will see 5 V of burden at 20 mA. This is a big chunk of the available headroom for our 12 V system. Are there alternative approaches? Obviously we can increase the C and reduce the R, but apparently this could have EMC implications?
Thanks,
Scott