1. I made a single-ended circuit by referring to the ad7626 data sheet.
The circuit is as follows.
2. I'm currently doing a good job ADC capturing signals on this circuit.
3. But the heat is about 50 degrees in ada4899-1.
4. I use the Precision ADC Drive Tool on the analog homepage, so use 100 ohms as shown below.
5. Even if I switch to 100 ohms, the heat keeps coming to ada4899-1.
6. Is there a problem with the ada4899-1 having a heat of about 50 degrees in the ad7626 single-ended circuit?
7. What's the way to solve this?
8. And why is the result of the single-ended circuit of AD7626 data sheet different from the Precision ADC Driver Tool of the Analyst homepage?
- Why is Datasheet telling me to use 590 ohms and Precision ADC Driver Tool not to use 590 ohms?