Hi,
I would make sure that absolute maximum voltage of SDA is "Digital Output Voltage to GND", Is it correct?
Best regards
AD7995
Production
The AD7991 / AD7995 / AD7999 are 12-/10-/8-bit, low power, successive approximation ADCs with an I2C®-compatible interface. Each part operates from...
Datasheet
AD7995 on Analog.com
Hi,
I would make sure that absolute maximum voltage of SDA is "Digital Output Voltage to GND", Is it correct?
Best regards
Hi kshigemori281 ,
Please refer to page 12, specifically on Table 7 for its Pin Function. It states that the SDA is a bidirectional pin. Meaning, it can be used as its input or its output.
Also, please refer to its absolute maximum rating on page 11, the maximum digital input voltage would be having a range from -0.3 V to +7 V. While the maximum digital output voltage would be having a range of -0.3 V to VDD + 0.3 V. So, you should consider what configuration are you going to use so that it would not exceed its maximum rating.
Regards,
Jo