AD7791
Production
The AD7790/AD7791 are low-power, complete analog front ends for low frequency measurement applications. The device consumes 65 µA of current typically...
Datasheet
AD7791 on Analog.com
AD7780
Production
The AD7780 is a complete low power front-end solution for bridge sensor products, including weigh scales, strain gages, and pressure sensors. It contains...
Datasheet
AD7780 on Analog.com
Hi everyone,
I'm trying to use a LTC2500 for temperature control of my device, but all the stuff I found on the internet is either confusing or not very helpful. Does anyone have tried / succeeded to do it ?
Here is my schematic :
Hi France , I would like to understand the application of your device, so let me know: 1. the temperature range 2. the resolution you need (are you dealing a fluctuating temperature or a steady one?) The LTC2500 is a good choice because it is a Dual Output 32-BIT SAR ADC. Unfortunately, the software driver to support the Arduino for LTC2500 is unavailable.
I suggest you check the AD7780 and AD7791. The Linux drivers are available, and they are in high resolution applications.
Thank you.