Post Go back to editing

AD7327-EP Input Voltage dip

Category: Hardware
Product Number: AD7327-EP
Software Version: NA

Hi,

AD7327-EP usage configurations:

  1. External RC filter for each channel (R=200 ohms, C=680pF)
  2. CH5 to CH7, configured as DC channels and range are as follows:
  3. CH5 +/- 2.5V
  4. CH6 +/- 10V
  5. CH7 +/- 5V
  6. CLK is 6.6MHz
  7. CS low to CS low is 2.72us

Issue with CH5:

  1. Input voltage applied at CH5, 2.498 VDC from function generator
  2. ADC is configured to capture 8 samples from the same channel (CH5)
  3. The datasheet specifies Track mode starts from 14th rising edge clock cycle.
  4. During this there is a dip in the input voltage observed (Waveforms attached). And it is happening for all the 8 samples. The input is constant 2.48VDC and not changing at all.
  5. Why is this behavior ? any reason ?. Is the internal sampling capacitor discharged every time ?
  6. How much time is required for Input to reach steady state?

 

Details on Waveforms:

  1. The labels are provided to indicate the signal
  2. The VCH5 is the voltage at the input of ADC CH5, Exactly probed across the external Capacitor.

 

Thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.