A few questions about the MAX11043:
- Instead of using the external UP/DOWN or DACSTEP pins, I can simply write to the DAC registers over SPI and leave those pins unconnected. Correct?
- The datasheet indicates there is a 12-bit DAC and two 8-bit DACs. I see the 12-bit DAC output pin, but how does one use the 8-bit DACs? Can all three DACs be used at the same time?
- The datasheet recommends sending the same clock used for SPI to the external clock input for best performance. What happens if I use the internal osc instead, with the SPI clock being separate and presumably a different rate?
Edit Notes
added tag[edited by: JCCillion at 9:39 AM (GMT -4) on 13 Jul 2023]